about ADC sampling clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

about ADC sampling clock

跳至解决方案
1,501 次查看
goto11
Contributor III

hello,Community

Can I change the ADC sampling clock during operation?
Are there any precautions when making changes?

best regards

Goto

标签 (1)
0 项奖励
回复
1 解答
1,370 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Goto

for clock usage one can look at Figure 14-2. Timing

i.MX 7Dual Applications Processor Reference Manual

Seems it is possible to change clock during operation,

valid data will be on next conversion cycle.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,371 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Goto

for clock usage one can look at Figure 14-2. Timing

i.MX 7Dual Applications Processor Reference Manual

Seems it is possible to change clock during operation,

valid data will be on next conversion cycle.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,370 次查看
goto11
Contributor III

hello,

Table 93. Recommended operating conditions for 12-bit ADC in .MX 7 Dual Family of Applications Processors Datasheet
Is it OK to make the RIEXT value larger than 250Ω (for example, from several kΩ to dozens of kΩ) when FCLK and FSOC are operated at close Min values?

What kind of problems will occur if the resistance value is increased?

best regards

Goto

0 项奖励
回复
1,370 次查看
igorpadykov
NXP Employee
NXP Employee

for new questions recommended to create new thread.

Best regards
igor

0 项奖励
回复