hi,everyone
I have a problem about mfgtool,our evn is :
linux 3.10.53 ,imx6q sabresd mfgtool is imx-3.10.53_1.1.0_ga-mfg-tools
(1) we use 2GB DDR (64bit) for our system,and mfgtool can success to run.
(2) we take down 2 DDR chip (for 32 bit 1GB DDR),and we change the DDR parameter,and ddr stress test is OK,but we fail to run mfgtool,the mfgtool stop run after starting UTP,the log is as follow:
wm8962-supply: disabling
regulator-dummy: disabling
imx mcc test is registered.
g_mass_storage gadget: Mass Storage Function, version: 2009/09/11
g_mass_storage gadget: Number of LUNs=1
lun0: LUN: removable file: (no medium)
g_mass_storage gadget: Mass Storage Gadget, version: 2009/09/11
g_mass_storage gadget: g_mass_storage ready
input: gpio-keys.26 as /devices/soc0/gpio-keys.26/input/input1
snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:06:17 UTC (377)
ALSA device list:
#0: imx-hdmi-soc
Freeing unused kernel memory: 324K (80bf6000 - 80c47000)
Starting UTP
uuc 0.5 [built Jan 5 2015 14:47:13]
UTP: Waiting for device to appear
UTP: file/device node /dev/utp already exists
cpu_id is 0
(stop here)
(3) we use the same uboot,kernel,dtb,fs (for mfgtool) in 2GB DDR,and the mfgtool is OK,so I think the filesystem for mfgtool (fsl-image-mfgtool-initramfs-imx6qdlsolo.cpio.gz.u-boot) must match 2GB DDR.
how can I use the mfgtool in 32bit 1GB DDR (in imx6q sabresd)?
or how can I compile the yocto for 32bit 1GB ddr for mfgtool?
can you give me a filesystem for mfgtool in 32 bit DDR (in imx6q sabresd)?
Is everyone can help me?
Best wishes!
Solved! Go to Solution.
hi,igor
I have solve the problem, It is a hardware problem,the pin of id in otg was pull down by a resistance.so that the otg cannot be a slave device.and th UTP cannot receive the windows's command.
thanks for your help!
Best regards
Hi wang
you are right: for using mfgtool with 32bit 1GB DDR it is necessary to rebuild
mfgtools with modified uboot/.. mx6q_xxx.cfg file. For rebuilding
please refer to attached Yocto Guide sect.6.2 The Manufacturing Tool, MFGTool.
Regarding 32-bit ddr configuration one can also look at sect.5 Enabling Solo Emulation
attached i.MX_Linux_User's_Guide.pdf.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hi igorpadykov,
thanks for your replay.
(1) you are right: for using mfgtool with 32bit 1GB DDR it is necessary to rebuild
mfgtools with modified uboot/.. mx6q_xxx.cfg file. For rebuilding
please refer to attached Yocto Guide sect.6.2 The Manufacturing Tool, MFGTool.
According to your suggestion,I modify the source code in "fsl-arm-yocto-bsp/build-mfg/tmp/work/imx6qsabresd-poky-linux-gnueabi/u-boot-imx-mfgtool/2014.04-r0/git/board/freescale/imx/ddr/mx6q_4x_mt41j128.cfg" for 32bit ddr, and then compile the mfgtools :
bitbake -c compile -f fsl-image-mfgtool-initramfs
bitbake fsl-image-mfgtool-initramfs
compile the uboot (mx6qsabresd):
bitbake -c compile -f u-boot-mfgtool
bitbake u-boot-mfgtool
but I still can not run mfgtool successfully.always stop at:
UTP: Waiting for device to appear
UTP: file/device node /dev/utp already exists
cpu_id is 0
(2)Regarding 32-bit ddr configuration one can also look at sect.5 Enabling Solo Emulation
attached i.MX_Linux_User's_Guide.pdf.
compile the uboot for 32bit ddr: (mx6solosabreauto)
MACHINE=imx6solosabreauto bitbake u-boot-imx-mfgtool
and then I found this ubootXX.imx can not be load,I get nothing in console.
Could you tell me in detail ?
Best wishes!
Hi wang
had you changed uboot/..configs/board_file.h parameters
for custom board, like:
define PHYS_SDRAM_SIZE
~igor
hi,igorpadykov
(1) this is my log:
---------------------------
U-Boot 2014.04 (Aug 12 2015 - 14:13:01)
CPU: Freescale i.MX6Q rev1.2 at 792 MHz
CPU: Temperature 27 C, calibration data: 0x5814ee69
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 1 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
MMC: no card present
MMC init failed
Using default environment
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
Found PFUZE100 deviceid=10,revid=11
MMC: no card present
mmc1(part 0) is current device
Net: Phy not found
PHY reset timed out
FEC [PRIME]
Warning: failed to set MAC address
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot: 0
Kernel image @ 0x12000000 [ 0x000000 - 0x5105d0 ]
## Loading init Ramdisk from Legacy Image at 12c00000 ...
Image Name: fsl-image-mfgtool-initramfs-imx6
Image Type: ARM Linux RAMDisk Image (gzip compressed)
Data Size: 7304221 Bytes = 7 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 18000000
Booting using the fdt blob at 0x18000000
Using Device Tree in place at 18000000, end 1800f69c
switch to ldo_bypass mode!
Starting kernel ...
Booting Linux on physical CPU 0x0
Linux version 3.10.53 (wangzg@localhost.localdomain) (gcc version 4.6.3 (crosstool-NG linaro-1.13.1-2012.03-20120326 - Linaro GCC 2012.03) ) #3 SMP Thu Jul 30 19:02:35 CST 2015
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Freescale i.MX6 Quad/DualLite (Device Tree), model: Freescale i.MX6 Quad SABRE Smart Device Board
cma: CMA: reserved 320 MiB at 3c000000
Memory policy: ECC disabled, Data cache writealloc
PERCPU: Embedded 8 pages/cpu @81513000 s8768 r8192 d15808 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260096
Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= enable_wait_mode=off
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 1024MB = 1024MB total
Memory: 690552k/690552k available, 358024k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
vmalloc : 0xc0800000 - 0xff000000 (1000 MB)
lowmem : 0x80000000 - 0xc0000000 (1024 MB)
modules : 0x7f000000 - 0x80000000 ( 16 MB)
.text : 0x80008000 - 0x80bf5554 (12214 kB)
.init : 0x80bf6000 - 0x80c47240 ( 325 kB)
.data : 0x80c48000 - 0x80c98940 ( 323 kB)
.bss : 0x80c98940 - 0x80cfaf5c ( 394 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
Hierarchical RCU implementation.
NR_IRQS:16 nr_irqs:16 16
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1048576 B
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms
CPU identified as i.MX6Q, silicon rev 1.2
Console: colour dummy device 80x30
Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x80623fb0 - 0x80624008
CPU1: Booted secondary processor
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
CPU2: Booted secondary processor
CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
CPU3: Booted secondary processor
CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
Brought up 4 CPUs
SMP: Total of 4 processors activated (6324.22 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
pinctrl core: initialized pinctrl subsystem
regulator-dummy: no parameters
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
Use WDOG2 as reset source
syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered
vdd1p1: 800 <--> 1375 mV at 1100 mV
vdd3p0: 2800 <--> 3150 mV at 3000 mV
vdd2p5: 2000 <--> 2750 mV at 2400 mV
cpu: 725 <--> 1450 mV
vddpu: 725 <--> 1450 mV
vddsoc: 725 <--> 1450 mV
syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered
syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
bio: create slab <bio-0> at 0
mxs-dma 110000.dma-apbh: initialized
usb_otg_vbus: 5000 mV
usb_h1_vbus: 5000 mV
wm8962-supply: no parameters
mipi_dsi_pwr_on: no parameters
sensor-supply: 3300 mV
i2c-core: driver [max17135] using legacy suspend method
i2c-core: driver [max17135] using legacy resume method
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c i2c-0: IMX I2C adapter registered
i2c i2c-1: IMX I2C adapter registered
imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_GPIO_3 already requested by 20e0000.iomuxc; cannot claim for 21a8000.i2c
imx6q-pinctrl 20e0000.iomuxc: pin-139 (21a8000.i2c) status -22
imx6q-pinctrl 20e0000.iomuxc: could not request pin 139 on device 20e0000.iomuxc
imx-i2c 21a8000.i2c: Error applying setting, reverse things back
imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_GPIO_3 already requested by 20e0000.iomuxc; cannot claim for 21a8000.i2c
imx6q-pinctrl 20e0000.iomuxc: pin-139 (21a8000.i2c) status -22
imx6q-pinctrl 20e0000.iomuxc: could not request pin 139 on device 20e0000.iomuxc
imx-i2c 21a8000.i2c: Error applying setting, reverse things back
imx-i2c 21a8000.i2c: can't get/select pinctrl
imx-i2c: probe of 21a8000.i2c failed with error -22
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Initialized.
cfg80211: Calling CRDA to update world regulatory domain
pureg-dummy: no parameters
Switching to clocksource mxc_timer1
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 4, 65536 bytes)
TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
TCP: reno registered
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 7128K (82c01000 - 832f7000)
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
imx6_busfreq busfreq.16: DDR medium rate not supported.
Bus freq driver module loaded
futex hash table entries: 1024 (order: 4, 65536 bytes)
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.
fuse init (API version 7.22)
msgmni has been set to 2002
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: WEIM driver registered.
ldb ldb.14: dual mode
ldb ldb.14: split mode or dual mode, ignoring second output
mxc_mipi_dsi 21e0000.mipi: i.MX MIPI DSI driver probed
MIPI DSI driver module loaded
mxc_sdc_fb fb.29: registered mxc display driver ldb
imx-ipuv3 2800000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
Console: switching to colour frame buffer device 128x48
mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1
fbcvt: 1920x1080@60: CVT Name - 2.073M9
mxc_sdc_fb fb.30: registered mxc display driver hdmi
mxc_sdc_fb fb.31: registered mxc display driver lcd
mxc_sdc_fb fb.31: ipu0-di0 already in use
mxc_sdc_fb: probe of fb.31 failed with error -16
ldb ldb.14: LVDS channel1 is not online
mxc_sdc_fb fb.32: NO mxc display driver found!
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: loaded firmware 1.1
imx-sdma 20ec000.sdma: initialized
pfuze100-regulator 1-0008: Full lay: 1, Metal lay: 1
pfuze100-regulator 1-0008: FAB: 0, FIN: 0
pfuze100-regulator 1-0008: pfuze100 found.
SW1AB: 300 <--> 1875 mV at 1150 mV
SW1C: 300 <--> 1875 mV at 1175 mV
SW2: 800 <--> 3300 mV at 3300 mV
SW3A: 400 <--> 1975 mV at 1500 mV
SW3B: 400 <--> 1975 mV at 1500 mV
SW4: 800 <--> 3300 mV at 3150 mV
SWBST: 5000 <--> 5150 mV at 5000 mV
VSNVS: 1000 <--> 3000 mV at 3000 mV
VREFDDR: 750 mV
VGEN1: 800 <--> 1550 mV at 1500 mV
VGEN2: 800 <--> 1550 mV at 1500 mV
VGEN3: 1800 <--> 3300 mV at 2800 mV
VGEN4: 1800 <--> 3300 mV at 1800 mV
VGEN5: 1800 <--> 3300 mV at 3000 mV
VGEN6: 1800 <--> 3300 mV at 3300 mV
Serial: IMX driver
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
console [ttymxc0] enabled
21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX
21f4000.serial: ttymxc4 at MMIO 0x21f4000 (irq = 62) is a IMX
serial: Freescale lpuart driver
imx sema4 driver is registered.
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_KEY_COL1 already requested by 21f4000.serial; cannot claim for 2008000.ecspi
imx6q-pinctrl 20e0000.iomuxc: pin-128 (2008000.ecspi) status -22
imn6d mr25h256, expected m25p32
K25p80 spi32766.0: mr25h256 (32
usbcore: registered new interface driver usb-storage
ci_hdrc ci_hdrc.0: EHCI Host Controller
ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
ci_hdrc ci_hdrc.1: doesn't support gadget
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 2
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
mousedev: PS/2 mouse device common for all mice
egalax_ts 1-0004: Failed to read firmware version
egalax_ts: probe of 1-0004 failed with error -5
input: max11801_ts as /devices/soc0/soc.1/2100000.aips-bus/21a4000.i2c/i2c-1/1-0048/input/input0
i2c-core: driver [isl29023] using legacy suspend method
i2c-core: driver [isl29023] using legacy
rmxc_v4l2_output v4l2_out.37: V4L2 device registered as video17
mxc_v4l2_output v4l2_out.37: V4L2 device registered as video18
mxc_v4l2_output v4l2_out.37: V4L2 device registered as video19
i2c-core: driver [mag3110] using legacy suspend method
i2c-core: driver [mag3110] using legacy resume method
mma8451 0-001c: read chip ID 0x1 is not equal to 0x1a or 0x2a!
mma8451: probe of 0-001c failed with error -22
imx2-wdt 20c0000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
watchdog: Software Watchdog: cannot register miscdev on minor=130 (err=-16).
watchdog: Software Watchdog: a legacy watchdog module is probably present.
softdog: Software Watchdog Timer: 0.08 initialized. soft_noboot=0 soft_margin=60 sec soft_panic=0 (nowayout=0)
cpuidle: using governor ladder
cpuidle: using governor menu
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc1: no vqmmc regulator found
mmc1: no vmmc regulator found
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
mmc2: no vqmmc regulator found
mmc2: no vmmc regulator found
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
mmc3: no vqmmc regulator found
mmc3: no vmmc regulator found
mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
Galcore version 5.0.11.25762
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
mxc_asrc 2034000.asrc: mxc_asrc registered
mxc_vpu 2040000.vpu: VPU initialized
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
wm8962 0-001a: Failed to read ID register
wm8962: probe of 0-001a failed with error -5
imx-wm8962 sound.27: failed to find codec platform device
imx-wm8962: probe of sound.27 failed with error -22
imx-audio-hdmi sound-hdmi.28: hdmi-hifi <-> hdmi_audio.17 mapping ok
TCP: cubic registered
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
VGEN3: disabling
VGEN2: disabling
VGEN1: disabling
SWBST: disabling
SW4: disabling
wm8962-supply: disabling
regulator-dummy: disabling
imx mcc test is registered.
g_mass_storage gadget: Mass Storage Function, version: 2009/09/11
g_mass_storage gadget: Number of LUNs=1
lun0: LUN: removable file: (no medium)
g_mass_storage gadget: Mass Storage Gadget, version: 2009/09/11
g_mass_storage gadget: g_mass_storage ready
input: gpio-keys.26 as /devices/soc0/gpio-keys.26/input/input1
snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0)
ALSA device list:
#0: imx-hdmi-soc
Freeing unused kernel memory: 324K (80bf6000 - 80c47000)
Starting UTP
uuc 0.5 [built Aug 11 2015 18:01:57]
UTP: Waiting for device to appear
UTP: file/device node /dev/utp already exists
cpu_id is 0
----------------------------------
(2) and I think I don't need to modify "define PHYS_SDRAM_SIZE" in mx6qsabresd board,
$ grep -r "PHYS_SDRAM_SIZE" ./
./drivers/video/mb86r0xgdc.c: pGD->frameAdrs = PHYS_SDRAM + PHYS_SDRAM_SIZE - VIDEO_MEM_SIZE;
./include/configs/mx6sxsabreauto.h:#define PHYS_SDRAM_SIZE SZ_2G
./include/configs/pm9261.h:#define PHYS_SDRAM_SIZE 0x04000000 /* 64 megs */
./include/configs/vf610twr.h:#define PHYS_SDRAM_SIZE (128 * 1024 * 1024)
./include/configs/mx53loco.h:#define PHYS_SDRAM_SIZE (gd->ram_size)
./include/configs/mx6sxsabresd.h:#define PHYS_SDRAM_SIZE SZ_1G
./include/configs/pm9263.h:#define PHYS_SDRAM_SIZE 0x04000000 /* 64 megs */
./include/configs/titanium.h:#define PHYS_SDRAM_SIZE (512 << 20)
./include/configs/zmx25.h:#define PHYS_SDRAM_SIZE 0x04000000 /* 64 megs */
./include/configs/zmx25.h:#define CONFIG_SYS_MEMTEST_END (PHYS_SDRAM + PHYS_SDRAM_SIZE)
./include/configs/m53evk.h:#define PHYS_SDRAM_SIZE (gd->ram_size)
./include/configs/kzm9g.h:#define PHYS_SDRAM_SIZE (512 * 1024 * 1024)
./include/configs/kzm9g.h:#define CONFIG_SYS_SDRAM_SIZE (PHYS_SDRAM_SIZE - CONFIG_SDRAM_OFFSET_FOR_RT)
./include/configs/jadecpu.h:#define PHYS_SDRAM_SIZE 0x08000000 /* 128 megs */
./include/configs/jadecpu.h:#define CONFIG_SYS_MEMTEST_END (PHYS_SDRAM + PHYS_SDRAM_SIZE)
./include/configs/mx6sx_arm2.h:#define PHYS_SDRAM_SIZE SZ_1G
./include/configs/u8500_href.h:#define PHYS_SDRAM_SIZE_1 0x20000000 /* 512 MB */
./include/configs/mx53smd.h:#define PHYS_SDRAM_SIZE (PHYS_SDRAM_1_SIZE + PHYS_SDRAM_2_SIZE)
./include/configs/mx6slevk.h:#define PHYS_SDRAM_SIZE SZ_1G
./include/configs/cgtqmx6eval.h:#define PHYS_SDRAM_SIZE (1u * 1024 * 1024 * 1024)
./include/configs/pm9g45.h:#define PHYS_SDRAM_SIZE 0x08000000 /* 128 megs */
./include/configs/mx53ard.h:#define PHYS_SDRAM_SIZE (PHYS_SDRAM_1_SIZE + PHYS_SDRAM_2_SIZE)
I think similar problem is discussed below and
problem was in host computer administrator rights
MFGTool not working for i.MX6 DualLite CPU Card
please try with WinXP 32 bit computer.
Also you wrote one time about "mx6qsabresd", another time
about "MACHINE=imx6solosabreauto"
what exactly your board is based on :
solosabreauto or sabresd ? One should not mix these
settings since these are different boards and configurations.
So if your board is based on mx6qsabresd, then you
should use only configurations for mx6qsabresd.
One can look at imx6solosabreauto configurations just for
reference and modify mx6qsabresd files, if necessary.
Best regards
igor
hi,igor
I have solve the problem, It is a hardware problem,the pin of id in otg was pull down by a resistance.so that the otg cannot be a slave device.and th UTP cannot receive the windows's command.
thanks for your help!
Best regards
Thanks,I meet the same problem and solve it with your method。
王工,你好。
为了布线的方便,我这边也打算拿掉2片DDR3(for 32 bit 1GB DDR)。想问下你,板上的这两个DDR3(片选信号)都接到DRAM_CS0上, 还是两片DDR3(片选信号)分别接到DRAM_CS0和DRAM_CS1上呢?
应该都接到cs0吧