ZQ calibration on i.MX53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ZQ calibration on i.MX53

1,307 Views
j_thiesen
Contributor I

Hello,

In application note AN4466, it states that the following calibration sequences needs to be run when bring up a board.

• ZQ calibration

• Write leveling calibration

• DQS gating calibration

• Read data DQS calibration

• Write data DQS calibration

We have the DDR3 stress test tool and have applied it to our current i.MX53 design.  When we run the calibration test we see that we get strobe, read, and write delays.  The question we have is does the DDR stress test tool run the ZQ calibration and the write leveling when it runs the calibration routine or do we have to this separately?

Labels (2)
0 Kudos
Reply
4 Replies

932 Views
j_thiesen
Contributor I

If its not too late to ask a follow up a programmer here has asked: Are there code examples for the ZQ and write leveling test?

0 Kudos
Reply

932 Views
j_thiesen
Contributor I

Thank you very much.

0 Kudos
Reply

932 Views
Yuri
NXP Employee
NXP Employee

   The following may be useful :

i.MX53 Memory Calibration Script (AN4466)

Regards,

Yuri.

0 Kudos
Reply

932 Views
igorpadykov
NXP Employee
NXP Employee

Hi J

i.MX53 ddr tester tool (below link) does not have calibration/leveling routines,

one needs to implement them separately

DDR_STRESS_TESTER_FOR_MX51_MX53 : DDR Stress tester kit

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply