Yocto related error?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto related error?

Jump to solution
4,905 Views
bandarulavanya
Contributor V

Hi all,

when i am doing bitbake fsl-image-machine-test or bitbake linux-imx i am getting like following

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

ERROR: Function failed: Fetcher failure: Fetch command failed with exit code 128, output:

Cloning into '/home/Lavanya/Workdir/Projects/yacto/Sources/yocto/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/glibc-initial/2.20-r0/git'...

done.

fatal: cannot process 'refs/remotes/origin/hjl/pthread' and 'refs/remotes/origin/hjl/pthread/2.21' at the same time

fatal: The remote end hung up unexpectedly

ERROR: Logfile of failure stored in: /home/Lavanya/Workdir/Projects/yacto/Sources/yocto/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/glibc-initial/2.20-r0/temp/log.do_unpack.32385

Log data follows:

| DEBUG: Executing python function do_unpack

| DEBUG: Executing python function base_do_unpack

| DEBUG: Running export SSH_AGENT_PID="1877"; export SSH_AUTH_SOCK="/tmp/keyring-EL0yw2/ssh"; export PATH="/home/Lavanya/Workdir/Projects/yacto/Sources/yocto/build/tmp/sysroots/i686-linux/usr/bin/arm-poky-linux-gnueabi.gcc-cross-initial-arm:/home/Lavanya/Workdir/Projects/yacto/Sources/yocto/sources/poky/scripts:/home/Lavanya/Workdir/Projects/yacto/Sources/yocto/build/tmp/sysroots/i686-linux/usr/bin/arm-poky-linux-gnueabi:/home/Lavanya/Workdir/Projects/yacto/Sources/yocto/build/tmp/sysroots/imx6_fs_wcam/usr/bin/crossscripts:/home/Lavanya/Workdir/Projects/yacto/Sources/yocto/build/tmp/sysroots/i686-linux/usr/sbin:/home/Lavanya/Workdir/Projects/yacto/Sources/yocto/build/tmp/sysroots/i686-linux/usr/bin:/home/Lavanya/Workdir/Projects/yacto/Sources/yocto/build/tmp/sysroots/i686-linux/sbin:/home/Lavanya/Workdir/Projects/yacto/Sources/yocto/build/tmp/sysroots/i686-linux/bin:/home/Lavanya/Workdir/Projects/yacto/Sources/yocto/sources/poky/scripts:/home/Lavanya/Workdir/Projects/yacto/Sources/yocto/sources/poky/bitbake/bin:/home/Lavanya/bin:/home/Lavanya/bin:/usr/local/arm_linux_4.2/bin:/usr/local/arm_linux_4.2/bin:/usr/local/arm_linux_4.2/bin:/usr/local/arm_linux_4.2/bin:/usr/local/arm_linux_4.2/bin:/usr/local/arm_linux_4.2/bin:/usr/local/arm_linux_4.2/bin:/usr/local/arm_linux_4.2/bin:/usr/lib/lightdm/lightdm:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games"; export HOME="/home/Lavanya"; git -c core.fsyncobjectfiles=0 clone -s -n /home/Lavanya/Workdir/Projects/yacto/Sources/yocto/downloads//git2/sourceware.org.git.glibc.git/ /home/Lavanya/Workdir/Projects/yacto/Sources/yocto/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/glibc-initial/2.20-r0/git/

| DEBUG: Python function base_do_unpack finished

| DEBUG: Python function do_unpack finished

| ERROR: Function failed: Fetcher failure: Fetch command failed with exit code 128, output:

| Cloning into '/home/Lavanya/Workdir/Projects/yacto/Sources/yocto/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/glibc-initial/2.20-r0/git'...

| done.

| fatal: cannot process 'refs/remotes/origin/hjl/pthread' and 'refs/remotes/origin/hjl/pthread/2.21' at the same time

| fatal: The remote end hung up unexpectedly

|

ERROR: Task 497 (/home/Lavanya/Workdir/Projects/yacto/Sources/yocto/sources/poky/meta/recipes-core/glibc/glibc-initial_2.20.bb, do_unpack) failed with exit code '1'

NOTE: Tasks Summary: Attempted 196 tasks of which 4 didn't need to be rerun and 1 failed.

Waiting for 0 running tasks to finish:

Summary: 1 task failed:

  /home/Lavanya/Workdir/Projects/yacto/Sources/yocto/sources/poky/meta/recipes-core/glibc/glibc-initial_2.20.bb, do_unpack

Summary: There were 5 WARNING messages shown.

Summary: There was 1 ERROR message shown, returning a non-zero exit code.

How can i solve this issue ....

Thanks & Regards,

Lavanya

1 Solution
4,026 Views
bandarulavanya
Contributor V

Hi Yuri Muhin,

Thank you, i solved the issue

in downloads folder "downloads/git2/sourceware.org.git.glibc.git/refs/heads/hjl/pthread"

after deleting 2.21 file i am not getting this error

Thanks & Regards,

Lavanya

View solution in original post

2 Replies
4,026 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Please describe in more details the issue - how to reproduce it.

Have a great day,

Yuri

0 Kudos
Reply
4,027 Views
bandarulavanya
Contributor V

Hi Yuri Muhin,

Thank you, i solved the issue

in downloads folder "downloads/git2/sourceware.org.git.glibc.git/refs/heads/hjl/pthread"

after deleting 2.21 file i am not getting this error

Thanks & Regards,

Lavanya