Dear friends ,
I am setting up a host for L5.4... yocto project. Based on the document, I should install package python, pylint3 and rsnc. When I install them, the installer say install pynthon-is-pynth2, git, and pylint should be installed instead of these specified in document . It also say that the package Rsnc can not be located. Is rsnc a typo? Is rsnc should be rsync instead?
thank you
Hai
Dear joan
Switched to 18.04, rsnc still can not be found。I tried to do the repo sync, errors occured. Attanched is a sanpshot.
the following is the error message.
fatal: unable to access 'https://github.com/meta-rust/meta-rust/': Failed to connect to github.com port 443: Connection timed out
thank you
Hai
this is your network connection issue, you need check your network and try again, before you building, don't forget install all of packages in the chapter 3 Host Setup and chapter 1.2.1. Ubuntu and Debian of
"https://www.yoctoproject.org/docs/3.0/ref-manual/ref-manual.html#ubuntu-packages"
if you forget install something, I suggest that you delete the build folder, install first, then build again