Board: imx6qsabresd
host: ubuntu 12.04
FS: yocto project 1.5 (Dora)
Description:
When i try to compile application using poky toolchain installed via meta-toolchain, i am getting below linker errors. Please let me know how can i fix this
ERROR Log:
-------------------
/opt/poky/1.4.3/sysroots/i686-pokysdk-linux/usr/libexec/armv7a-vfp-neon-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.7.2/ld: cannot find /lib/libc.so.6
/opt/poky/1.4.3/sysroots/i686-pokysdk-linux/usr/libexec/armv7a-vfp-neon-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.7.2/ld: cannot find /usr/lib/libc_nonshared.a
/opt/poky/1.4.3/sysroots/i686-pokysdk-linux/usr/libexec/armv7a-vfp-neon-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.7.2/ld: cannot find /lib/ld-linux-armhf.so.3
collect2: error: ld returned 1 exit status
Also,
While building multi-threaded gstreamer application, we are getting pthread linker errors as shown below:
ERROR Log:
-------------------
/opt/poky/1.4.3/sysroots/i686-pokysdk-linux/usr/libexec/armv7a-vfp-neon-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.7.2/ld: cannot find /lib/libpthread.so.0
/opt/poky/1.4.3/sysroots/i686-pokysdk-linux/usr/libexec/armv7a-vfp-neon-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.7.2/ld: cannot find /usr/lib/libpthread_nonshared.a
collect2: error: ld returned 1 exit status
Below is my code test.c:
-----------------------------------
#include <pthread.h>
#include <stdio.h>
/* this function is run by the second thread */
void *inc_x(void *x_void_ptr)
{
/* increment x to 100 */
int *x_ptr = (int *)x_void_ptr;
while(++(*x_ptr) < 100);
printf("x increment finished\n");
/* the function must return something - NULL will do */
return NULL;
}
int main()
{
int x = 0, y = 0;
/* show the initial values of x and y */
printf("x: %d, y: %d\n", x, y);
/* this variable is our reference to the second thread */
pthread_t inc_x_thread;
/* create a second thread which executes inc_x(&x) */
if(pthread_create(&inc_x_thread, NULL, inc_x, &x)) {
fprintf(stderr, "Error creating thread\n");
return 1;
}
/* increment y to 100 in the first thread */
while(++y < 100);
printf("y increment finished\n");
/* wait for the second thread to finish */
if(pthread_join(inc_x_thread, NULL)) {
fprintf(stderr, "Error joining thread\n");
return 2;
}
/* show the results - x is now 100 thanks to the second thread */
printf("x: %d, y: %d\n", x, y);
return 0;
}
Command used to build:
-----------------------------------
/opt/poky/1.4.3/sysroots/i686-pokysdk-linux/usr/bin/armv7a-vfp-neon-poky-linux-gnueabi/arm-poky-linux-gnueabi-gcc -L/opt/fsl-imx6-sysroot/lib -L/opt/fsl-imx6-sysroot/usr/lib -lpthread test.c
Hi Leonardo,
I am getting this error too when I try to compile GStreamer Sample Application. I did source the environment script.I am able to compile and run a HelloWorld.c Application.
Sample application is from Chapter 10. Your first application link. The makefile I am using is attached below,
Makefile:
------------------------------------------------------------------------------------------------------------------------------------
# define the C compiler to use
CC = /opt/poky/1.4+snapshot/sysroots/i686-pokysdk-linux/usr/bin/cortexa9hf-vfp-neon-poky-linux-gnueabi/arm-poky-linux-gnueabi-gcc
# define any compile-time flags
CFLAGS = -Wall -g
# define any directories containing header files other than /usr/include
INCLUDES = -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/include/glib-2.0 -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/lib/glib-2.0/include/ -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/include/gstreamer-0.10/ -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/include/libxml2
LFLAGS = -L/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/lib
# define any libraries to link into executable:
LIBS = -lglib-2.0 -lxml2 -lgstreamer-0.10 -lgobject-2.0 -lz -lgmodule-2.0 -lffi
# define the C source files
SRCS = hellogst.c
# define the C object files
OBJS = $(SRCS:.c=.o)
# define the executable file
MAIN = hellogst
.PHONY: depend clean
all: $(MAIN)
@echo Simple compiler named simple has been compiled
$(MAIN): $(OBJS)
$(CC) $(CFLAGS) $(INCLUDES) -o $(MAIN) $(OBJS) $(LFLAGS) $(LIBS)
# this is a suffix replacement rule for building .o's from .c's
.c.o:
$(CC) $(CFLAGS) $(INCLUDES) -c $< -o $@
clean:
$(RM) *.o *~ $(MAIN)
depend: $(SRCS)
makedepend $(INCLUDES) $^
------------------------------------------------------------------------------------------------------------------------------------
Compilation Error:
------------------------------
$ make
/opt/poky/1.4+snapshot/sysroots/i686-pokysdk-linux/usr/bin/cortexa9hf-vfp-neon-poky-linux-gnueabi/arm-poky-linux-gnueabi-gcc -Wall -g -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/include/glib-2.0 -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/lib/glib-2.0/include/ -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/include/gstreamer-0.10/ -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/include/libxml2 -c hellogst.c -o hellogst.o
/opt/poky/1.4+snapshot/sysroots/i686-pokysdk-linux/usr/bin/cortexa9hf-vfp-neon-poky-linux-gnueabi/arm-poky-linux-gnueabi-gcc -Wall -g -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/include/glib-2.0 -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/lib/glib-2.0/include/ -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/include/gstreamer-0.10/ -I/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/include/libxml2 -o hellogst hellogst.o -L/home/suman/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd/usr/lib -lglib-2.0 -lxml2 -lgstreamer-0.10 -lgobject-2.0 -lz -lgmodule-2.0 -lffi
/opt/poky/1.4+snapshot/sysroots/i686-pokysdk-linux/usr/libexec/cortexa9hf-vfp-neon-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.8.1/ld: cannot find /lib/libc.so.6
/opt/poky/1.4+snapshot/sysroots/i686-pokysdk-linux/usr/libexec/cortexa9hf-vfp-neon-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.8.1/ld: cannot find /usr/lib/libc_nonshared.a
/opt/poky/1.4+snapshot/sysroots/i686-pokysdk-linux/usr/libexec/cortexa9hf-vfp-neon-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/4.8.1/ld: cannot find /lib/ld-linux-armhf.so.3
collect2: error: ld returned 1 exit status
make: *** [hellogst] Error 1
This issue has been resolved after manually editing the libpthread.so and libc.so file generated during yocto build. These files point to /usr/lib i.e. host pc libraries instead of current directory[/build-fb/tmp/sysroots/imx6qsabresd/usr/lib] which was causing the problem.
Hi Suman Ranjan,
what do u mean with "manualy editing libpthread.so and libc.so file"? Using an hex editor.
I am running exactly into your same problem.
What is strange is that I can successfully compile QT applications with qt creator following the instruction in Setup QT Creator with Yocto Build
Thanks in advance,
i.
You are right. I changed my CFLAGS accordingly and it worked too.
Makefile:
SYSROOT_PATH=/home/suman/svndump/fsl-community-bsp/build-fb/tmp/sysroots/imx6qsabresd
# define any compile-time flags
#CFLAGS = -fPIC -Wall -Wextra -O2 -g # old CFLAG
CFLAGS="--sysroot=$(SYSROOT_PATH)" # New CFLAG fixes the problem