iMX8M Plus configured for Yocto on Variscite DART-MX8M-PLUS, booting from eMMC.
While starting the kernel it fails to ever finish booting as it loops, printing "IRQ eth_lpi not found" messages over and over. I suspect the issue might be with the device tree but do not know for certain and also do not know how this would be remedied.
Boot log is attached.
Thank you in advance for any guidance.
Solved! Go to Solution.
Hi, sorry to leave the post unanswered. I did resolve the issue;
Variscite responded to me with the following after I described the issue to them:
"The message you are reporting is just an expected harmless warning.
You may want to edit the device tree and remove the second ethernet here
https://github.com/varigit/linux-imx/blob/lf-6.1.y_var03/arch/arm64/boot/dts/freescale/imx8mp-var-da..."
Upon removing the &eqos and &fec blocks from the device tree, the warning message disappeared. Not sure why this seems to have prevented it from booting.
Hopefully this helps.
Hi @cygnus.
If you are a Variscite customer, please register and create a ticket in the Variscite customer portal, and provide more details about the carrier board you are using: https://varisciteportal.axosoft.com/
Thanks,
Eran