Hi Pratyush
in attached dts file usdhc1 is commented out, so only usdhc2 is
available. In this case numbering may change to /dev/mmcblk0p2,
please refer to attached Linux Guide Table 31. Linux uSDHC relationships.
Also recommended to check with oscilloscope if correct sd
interface and all 8 data lines are toggled.
Regarding :
>if we use our own customised zImage and dtb file the board hangs while booting showing last message "waiting for root >device /dev/mmcblk1p2". While same image was working fine with imx6 evk board(sdcard).
it is strange that it is working with imx6 evk board (as it has 4 bit sd interface)
while you made sd configuration for 8 bit.
In general one can debug it using AN4553 Using Open Source Debugging Tools for
Linux on i.MX Processors sect.8.1 Debugging the Kernel Boot Phase
http://www.nxp.com/files/32bit/doc/app_note/AN4553.pdf
and enabling early printk
https://community.nxp.com/thread/351167
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------