Yocto fslc-x11 without cursor/theme/...

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Yocto fslc-x11 without cursor/theme/...

1,422 次查看
woutervh
Contributor IV

I want my fslc-x11 image to be booted without xterm/pointer/...

The only thing I want to have, is a fullscreen visual of my own X11 application (GTK-based). How can I prevent my image to have matchbox + pointer + xterm +...?

标签 (4)
0 项奖励
回复
1 回复

1,094 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello  Wouter Vanhauwaert,

You could either edit the image recipe or the local.conf file of your build directory to add or remove packages as required. The limitation here would be how the packages are distributed.

You can find the packages and dependencies of the image on the image recipe. Additionally, you can see the packages available on the BSP by running:

$ bitbake -s

In order to prevent that it gets included on the image you may add on the conf/local.conf file:

IMAGE_INSTALL_remove += "package_name"

Please note that since Yocto is not meant for development it does not keep track of changes on the compiled files. If you remove a package your safest bet would be performing a clean and then baking the image again, so to make sure that the images is being built from scratch.

I hope this helps!

Regards,

0 项奖励
回复