Hello,
I'm trying to generate a working zImage 5.15.71 for my iMX6 solo lite.
I tried both of : imx_v7_defconfig and imx_v6_v7_defconfig
But the result is KO : it's stuck at Starting kernel
It works perfectly with kernel 5.15.11 but I didn't find any Yocto official manifest with this kernel version.
Can you please either provide a working .config or a manifest using 5.15.11
Thanks
Solved! Go to Solution.
Hi
The problem was that I was testing a kernel 5.10.72 with a device tree compiled from a 5.15.11 kernel.
So I solved the problem when I aligned the kernel AND the device tree versions.
Best regards,
Aïda
Hi
The problem was that I was testing a kernel 5.10.72 with a device tree compiled from a 5.15.11 kernel.
So I solved the problem when I aligned the kernel AND the device tree versions.
Best regards,
Aïda
Hello,
There is no official BSP for 5.15.11 kernel, and 5.15.71 does not work for MX6SL you need 5.10.72.
Regards
Hi
I just tried version 5.10.72+gitAUTOINC+06213bb011-
From the imx-5.10.35-2.0.0.xml manifest of imx-linux-hardknott. I used MACHINE=imx6qdlsabreauto
But it didn't work. It's still stuck at Starting Kernel
Best regards,
Aïda