Hi,
I have problem with downloading package with newest yocto for imx6:
WARNING: Failed to fetch URL http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-vpu-5.4.33.bin;fsl-eula=true, attempting MIRRORS if available
ERROR: Fetcher failure: Fetch command failed with exit code 4, output:
wget: unable to resolve host address 'www.nxp.com'
ERROR: Function failed: Fetcher failure for URL: 'http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-vpu-5.4.33.bin;fsl-eula=true'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/sp/fsl-release-bsp/build-mcd/tmp/work/imx6qsabresd-poky-linux-gnueabi/imx-vpu/1_5.4.33-r0/temp/log.do_fetch.1934
ERROR: Task 5067 (/home/sp/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/imx-vpu/imx-vpu_5.4.33.bb, do_fetch) failed with exit code '1'
How can I solve this?
Hi
While I could fetch the files mentioned above I still can not access xserver-xorg-video-imx-viv-5.0.11.p8.6.tar.gz requested by meta-freescale/recipes-graphics/xorg-driver/xf86-video-imxfb-vivante.inc
Regards
Max
I also have the same problem after running
bitbake linux-imx firmware-bcmdhd packagegroup-base packagegroup-fsl-tools-testapps
The first time I have 2 fetch failures:
imx-vpu-1_5.4.35_r0 and imx-lib-1_5.5-r0
But the 2nd time( 2 days later) only 1 failure:
imx-lib-1_5.5-r0
Would you please check your server a.s.a.p. and give me feedback when I can fetch such files without
any problem ?
BR
Xi
The link you provided doesn't work either. As both "www.nxp.com" and "www.freescale.com" both resolve to Akami's edge caches, maybe the problem is there. Regardless, we're stuck until the content either returns or someone can provide a mirror.
Hi,
I have problem with Ycoto Krogoth, I cannot fetch these files:
http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-lib-5.5.tar.gz
http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-vpuwrap-1.0.68.bin;fsl-eula=true
http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-parser-4.1.4.bin;fsl-eula=true
http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//kernel-module-imx-gpu-viv-5.0.11.p8.6.tar.gz
http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-vpu-5.4.35.bin;fsl-eula=true
http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-gpu-viv-5.0.11.p8.6-hfp.bin;fsl-eula=true
How can I solve that?
I have the same problem.....