Yocto build system

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Yocto build system

跳至解决方案
2,038 次查看
dhavalvadhar
Contributor IV

Hello All,

I am new to i.MX6 and it's build system Yocto. I have i.MX 6 sololite EVM.

To start with I read Freescale Yocto Project User's Guide.pdf. And using that I am able to build 'core-image-minimal' and boot the board with SD card using that generated images. But still I am not able to understand the Yocto build system completely. Can anyone here on this community help me with this?

Also, suggest me the documents to start with to understand i.MX6 like how to boot it with different boot devices etc.

Appreciate your quick reply.

Thanks,

Dhaval

标签 (4)
标记 (2)
0 项奖励
回复
1 解答
1,588 次查看
igorpadykov
NXP Employee
NXP Employee

HI Dhaval

one can start with:

https://community.freescale.com/docs/DOC-104266

Freescale Yocto Project main page

Linux on the i.MX6 sabre sd platform in a few commands

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
1,589 次查看
igorpadykov
NXP Employee
NXP Employee

HI Dhaval

one can start with:

https://community.freescale.com/docs/DOC-104266

Freescale Yocto Project main page

Linux on the i.MX6 sabre sd platform in a few commands

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,588 次查看
dhavalvadhar
Contributor IV

Thanks Igor for your quick reply. I will go through the documents you suggested.

0 项奖励
回复