Yocto build of core-image-base with kernel 3.10.9 for imx6slevk hangs after Starting kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto build of core-image-base with kernel 3.10.9 for imx6slevk hangs after Starting kernel

ソリューションへジャンプ
18,528件の閲覧回数
stephenharper
Contributor II

I am attempting to build images with a more recent kernel version (the default appears to be 3.0.35) for the i.MX6SoloLite Evalutation Kit and seem to be running into a few problems.

I have successfully run the pre-built images from L3.0.35_13.10.02 from an SD card on the i.MX6SLEVK.

I have been working largely from the directions found here: https://community.freescale.com/docs/DOC-94849

I am building on Ubuntu 12.04

Bitbake reports version 1.20.0

Yocto version 1.5 (dora)

My local.conf file in /fsl-community-bsp/build/conf/ is unmodified with the following exceptions:

Machine was changed to imx6slevk:

MACHINE ??= 'imx6slevk'

The following line was added to the bottom of the file:

PREFERRED_VERSION_linux-imx_mx6 = "3.10.9"

After syncing repos, cleaning out the /tmp diectory and running 'bitbake -c cleanstate linux-imx', running 'bitbake core-image-base' runs successfully with a few duplicate inclusion warnings but no errors and the following files are created in /fsl-community-bsp/build/tmp$ cd deploy/images/imx6slevk/:

core-image-base-imx6slevk-20140116230057.rootfs.ext3

core-image-base-imx6slevk-20140116230057.rootfs.sdcard

core-image-base-imx6slevk-20140116230057.rootfs.tar.bz2

core-image-base-imx6slevk.ext3

core-image-base-imx6slevk.sdcard

core-image-base-imx6slevk.tar.bz2

modules--3.10.9-r0-imx6slevk-20140116230057.tgz

modules-imx6slevk.tgz

README_-_DO_NOT_DELETE_FILES_IN_THIS_DIRECTORY.txt

u-boot.imx

u-boot-imx6slevk.imx

u-boot-imx6slevk-v2013.10-r0.imx

uImage

uImage--3.10.9-r0-imx6slevk-20140116230057.bin

uImage--3.10.9-r0-imx6sl-evk-20140116230057.dtb

uImage--3.10.9-r0-imx6sl-evk-ldo-20140116230057.dtb

uImage-imx6slevk.bin

uImage-imx6sl-evk.dtb

uImage-imx6sl-evk-ldo.dtb

Simply replacing the uImage on my currently working SD card from the L3.0.35_13.10.02 images (sudo dd if=uImage of=/dev/mmcblk0 bs=512 seek=2048 conv=fsync) results in the boot process getting to "Starting kernel" then hanging indefinitely. The same result also occurs when using the generated version of u-boot as well.

Interestingly though, simply using the generated core-image-base-imx6slevk.sdcard image ($ sudo dd if=core-image-base-imx6slevk.sdcard of=/dev/mmcblk0 bs=1M) also results in the same behavior.

I am a bit uncertain as to how my SD card should be partitioned for use with the Yocto images.

The partitions on the SD card with the L3.0.35_12.10.20 images (which run successfully) appear as such:

(with u-boot and the uImage dd'd to the unallocated space before mmcblk0p1)

Screenshot from 2014-01-17 13_11_44.png

The partitions on the SD card dd'd from the .sdcard image, however, appear like this:

(with the uImage, dtb and ldo-dtb on the fat partition and u-boot *presumablly?* on the unallocated space just before the fat partition)

Screenshot from 2014-01-17 13_12_38.png

My u-boot environmental variables for the L3.0.35_12.10.20 images with the uImage and u-boot from the Yocto build dd'd are as follows:

baudrate=115200

boot_fdt=try

bootargs_base=setenv bootargs console=ttymxc0,115200

bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait

bootcmd=run bootcmd_mmc

bootcmd_mmc=run bootargs_base bootargs_mmc;mmc dev 1;mmc read ${loadaddr} 0x800 0x4000;bootm

bootdelay=3

bootscript=echo Running bootscript from mmc ...; source

console=ttymxc0

ethact=FEC

ethaddr=00:04:9f:03:02:72

ethprime=FEC

fdt_addr=0x81000000

fdt_file=imx6sl-evk.dtb

fdt_high=0xffffffff

initrd_high=0xffffffff

ip_dyn=yes

loadaddr=0x80800000

loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};

loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}

loaduimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${uimage}

mmcargs=setenv bootargs console=${console},${baudrate} root=${mmcroot}

mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootm ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootm; else echo WARN: Cannot load the DT; fi; fi; else bootm; fi;

mmcdev=0

mmcpart=1

mmcroot=/dev/mmcblk0p1 rootwait rw

netargs=setenv bootargs console=${console},${baudrate} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp

netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${uimage}; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then bootm ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootm; else echo WARN: Cannot load the DT; fi; fi; else bootm; fi;

script=boot.scr

stderr=serial

stdin=serial

stdout=serial

uimage=uImage

My u-boot environmental variables for the .sdcard image are as follows:

baudrate=115200

boot_fdt=try

bootcmd=mmc dev ${mmcdev};mmc dev ${mmcdev}; if mmc rescan; then if run loadbootscript; then run bootscript; else if run loaduimage; then run mmcboot; else run netboot; fi; fi; else run netboot; fi

bootdelay=3

bootscript=echo Running bootscript from mmc ...; source

console=ttymxc0

ethact=FEC

ethaddr=00:04:9f:03:02:72

ethprime=FEC

fdt_addr=0x81000000

fdt_file=imx6sl-evk.dtb

fdt_high=0xffffffff

initrd_high=0xffffffff

ip_dyn=yes

loadaddr=0x82000000

loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};

loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}

loaduimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${uimage}

mmcargs=setenv bootargs console=${console},${baudrate} root=${mmcroot}

mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootm ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootm; else echo WARN: Cannot load the DT; fi; fi; else bootm; fi;

mmcdev=0

mmcpart=1

mmcroot=/dev/mmcblk0p2 rootwait rw

netargs=setenv bootargs console=${console},${baudrate} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp

netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${uimage}; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then bootm ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootm; else echo WARN: Cannot load the DT; fi; fi; else bootm; fi;

script=boot.scr

stderr=serial

stdin=serial

stdout=serial

uimage=uImage

My apologies for the large quantity of information but I figure that too much is better than not enough.

Any help in regards to what direction I should go or resources that might help would be greatly appreciated.

ラベル(3)
1 解決策
9,581件の閲覧回数
LeonardoSandova
Specialist I

Stephen

Follow the guide on imx/docs

meta-fsl-bsp-release.git - Freescale i.MX Yocto BSP Release Layer

These are the metadata layers released from freescale, doing all the work necessary to boot a 3.10.9 kernel.

Leo

元の投稿で解決策を見る

0 件の賞賛
返信
23 返答(返信)
8,824件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Hi Stephen,

I faced the same hang issue you described. Here is a way to fix it:

- Boot the board and enter into the U-boot prompt by pressing any key

- Then enter the following commands in the U-boot prompt:

=> setenv fdt_addr 0x88000000

=>setenv fdt_file imx6l-evk-ldo.dtb

=> reset

I have sent the fdt_addr fix to the U-boot list.

Regards,

Fabio Estevam

0 件の賞賛
返信
8,824件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Correction (the 'save' command must be given prior to resetting):

=> setenv fdt_addr 0x88000000

=> setenv fdt_file imx6l-evk-ldo.dtb

=> save

=> reset

0 件の賞賛
返信
8,825件の閲覧回数
leoschwab
Contributor III

Let's try again :-) ...

In general, LTIB images and Yocto-generated images aren't interchangeable.

Stephen Harper wrote:

[ ... ]

Simply replacing the uImage on my currently working SD card from the L3.0.35_13.10.02 images (sudo dd if=uImage of=/dev/mmcblk0 bs=512 seek=2048 conv=fsync) results in the boot process getting to "Starting kernel" then hanging indefinitely. The same result also occurs when using the generated version of u-boot as well.

That might have worked with an LTIB build, but not under Yocto.  U-Boot's scriptlets are doing a fatload of the uImage, which means it's interpreting the VFAT filesystem.  As such, you should be mounting the first partition, copying the uImage file over, then cleanly unmounting the partition.

Interestingly though, simply using the generated core-image-base-imx6slevk.sdcard image ($ sudo dd if=core-image-base-imx6slevk.sdcard of=/dev/mmcblk0 bs=1M) also results in the same behavior.

Okay, that is puzzling.  Have you changed the kernel .config file?

I am a bit uncertain as to how my SD card should be partitioned for use with the Yocto images.

The partitions on the SD card with the L3.0.35_12.10.20 images (which run successfully) appear as such:

(with u-boot and the uImage dd'd to the unallocated space before mmcblk0p1)

Screenshot from 2014-01-17 13_11_44.png

The partitions on the SD card dd'd from the .sdcard image, however, appear like this:

(with the uImage, dtb and ldo-dtb on the fat partition and u-boot *presumablly?* on the unallocated space just before the fat partition)

Screenshot from 2014-01-17 13_12_38.png

The latter arrangement is my experience with Yocto-generated images.  Partition 1 is a VFAT volume with a kernel ("uImage") and, in Dora builds, a compiled DTB file.  U-Boot reads the files directly.  Partition 2 is the ext3-formatted rootfs.

Schwab

0 件の賞賛
返信
8,824件の閲覧回数
stephenharper
Contributor II

This cleared up some of my partitioning questions. Thanks.

0 件の賞賛
返信
8,826件の閲覧回数
leoschwab
Contributor III

EDIT: Oops, never mind; I just now noticed the tell-tale environment variable values that tell me you're running the latest U-Boot.

Looks like you specified an updated kernel, but not an updated U-Boot which can handle DTS-enabled booting.  The following line may help you:

PREFERRED_PROVIDER_u-boot = "u-boot-fslc"

I stuck that in my conf/machine/machine-name.conf file, and things were much happier.

Note that this may not be all you need to do to get your board booting, but it's an essential step, since the old U-Boot knows nothing about DTS.  (And yes, you'll have to do your U-Boot porting work again; there have been a ton of changes since version 2009.08.)

Schwab

0 件の賞賛
返信
9,582件の閲覧回数
LeonardoSandova
Specialist I

Stephen

Follow the guide on imx/docs

meta-fsl-bsp-release.git - Freescale i.MX Yocto BSP Release Layer

These are the metadata layers released from freescale, doing all the work necessary to boot a 3.10.9 kernel.

Leo

0 件の賞賛
返信
8,826件の閲覧回数
stephenharper
Contributor II

Well this definitely seems to be the right direction to be going in. Thank you very much.

Everything seems to go very well up until do_rootfs which seems to fail with both core-image-base and core-image minimal with the following error:

| WARNING: exit code 1 from a shell command.

| ERROR: Function failed: do_rootfs (log file is located at /home/stephen.harper/fsl-community-bsp/build/tmp/work/imx6slevk-poky-linux-gnueabi/core-image-base/1.0-r0/temp/log.do_rootfs.3816)

ERROR: Task 7 (/home/stephen.harper/fsl-community-bsp/sources/poky/meta/recipes-core/images/core-image-base.bb, do_rootfs) failed with exit code '1'

NOTE: Tasks Summary: Attempted 2431 tasks of which 2428 didn't need to be rerun and 1 failed.

No currently running tasks (2430 of 2432)

Here is what appears to be the relevant portion of the log file:

Note: adding Smart RPM DB channel

Note: to be installed:  run-postinsts@cortexa9hf_vfp_neon packagegroup-core-boot@imx6slevk

Loading cache...

Updating cache...               ######################################## [100%]

Computing transaction...error: Can't install sysvinit-inittab-2.88dsf-r10@imx6slevk: no package provides /bin/bash

Saving cache...

WARNING: exit code 1 from a shell command.

ERROR: Function failed: do_rootfs (log file is located at /home/stephen.harper/fsl-community-bsp/build/tmp/work/imx6slevk-poky-linux-gnueabi/core-image-minimal/1.0-r0/temp/log.do_rootfs.8395)

The following files are generated after the failure:

modules--3.10.9-r0-imx6slevk-20140118002357.tgz    

u-boot-imx6slevk.imx                                

uImage-imx6slevk.bin

modules-imx6slevk.tgz                             

uImage                                             

uImage-imx6sl-evk.dtb

README_-_DO_NOT_DELETE_FILES_IN_THIS_DIRECTORY.txt 

uImage--3.10.9-r0-imx6slevk-20140118002357.bin     

uImage-imx6sl-evk-ldo.dtb

u-boot.imx                                         

uImage--3.10.9-r0-imx6sl-evk-20140118002357.dtb

u-boot-imx6slevk-2013.04-r0.imx                   

uImage--3.10.9-r0-imx6sl-evk-ldo-20140118002357.dtb

Sadly, it generates no .sdcard image nor rootfs.

Copying the uImage, uImage-imx6sl-evk.dtb (renamed imx6sl-evk.dtb), and uImage-imx6sl-evk-ldo.dtb (renamed imx6sl-evk-ldo.dtb) onto the boot partition of an SD card created from an existing .sdcard image (earlier kernel) continues to result in a hang at Starting kernel.

0 件の賞賛
返信
8,826件の閲覧回数
LeonardoSandova
Specialist I

Hi Stephen,

Can you try doing your setup on a new build folder? lets try first to avoid pollution from previous builds.

Leo

0 件の賞賛
返信
8,826件の閲覧回数
stephenharper
Contributor II

Thanks Leo.

I blew away everything and started fresh from scratch just to be sure this wasn't an issue.

For the sake of being thorough (and to possibly help anyone else who might come this way) here are the exact steps I am taking:

From an entirely clean home directory -


mkdir ~/bin

curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo

PATH=$PATH:~/bin

chmod a+x ~/bin/repo

mkdir fsl-community-bsp

cd fsl-community-bsp

repo init -u http://github.com/Freescale/fsl-community-bsp-platform -b dora

vim .repo/manifest.xml

(Added the following lines to manifest.xml)

<remote fetch="git://git.freescale.com/imx" name="fsl-release"/>

<project remote="fsl-release" name="meta-fsl-bsp-release" path="sources/meta-fsl-bsp-release" revision="dora_3.10.9-1.0.0" >

<copyfile src="imx/tools/fsl-setup-release.sh" dest="fsl-setup-release.sh"/>

</project>

(Then ESC, :wq)

repo sync

cp -r sources/meta-fsl-bsp-release/imx/meta-fsl-arm/conf/machine sources/meta-fsl-arm/conf

MACHINE=imx6slevk source setup-environment build

(Read/agree to EULA)

cd ..

source fsl-setup-release.sh -b build -e dfb

bitbake core-image-minimal

(or core-image-base, etc.)


Does this seem right to you Leo?

It is building at the moment. (Always very slow the first time) I will post results when complete.


0 件の賞賛
返信
8,826件の閲覧回数
LeonardoSandova
Specialist I

That is correct Stephen. To faster the fetching phase, make sure you are using the same downloads folder as previous built. In order words, DL_DIR variable should be the same on build_new/conf/local.conf and build_old/conf/local.conf.

0 件の賞賛
返信
8,826件の閲覧回数
stephenharper
Contributor II

Same result : (

Here is the output of running bitbake core-image-minimal after running the before-mentioned commands from a clean build environment:

WARNING: Duplicate inclusion for /home/stephen.harper/fsl-community-bsp/sources/poky/meta/recipes-bsp/u-boot/u-boot.inc in /home/stephen.harper/fsl-community-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2013.04.bbappend

WARNING: Unable to get checksum for linux-boundary SRC_URI entry defconfig: file could not be found#################  | ETA:  00:00:01

WARNING: Unable to get checksum for gpu-viv-bin-mx6q SRC_URI entry vg.pc: file could not be found#################### | ETA:  00:00:00

WARNING: Unable to get checksum for gpu-viv-bin-mx6q SRC_URI entry vg_x11.pc: file could not be found

Parsing recipes: 100% |###############################################################################################| ETA:  00:00:00

Parsing of 1365 .bb files complete (0 cached, 1365 parsed). 1758 targets, 160 skipped, 0 masked, 0 errors.

NOTE: Resolving any missing task queue dependencies

Build Configuration:

BB_VERSION        = "1.20.0"

BUILD_SYS         = "x86_64-linux"

NATIVELSBSTRING   = "Ubuntu-12.04"

TARGET_SYS        = "arm-poky-linux-gnueabi"

MACHINE           = "imx6slevk"

DISTRO            = "poky"

DISTRO_VERSION    = "1.5.1"

TUNE_FEATURES     = "armv7a vfp neon callconvention-hard cortexa9"

TARGET_FPU        = "vfp-neon"

meta             

meta-yocto        = "(nobranch):bee7e3756adf70edaeabe9d43166707aab84f581"

meta-oe           = "(nobranch):eb4563b83be0a57ede4269ab19688af6baa62cd2"

meta-fsl-arm      = "(nobranch):af392c22bf6b563525ede4a81b6755ff1dd2c1c6"

meta-fsl-arm-extra = "(nobranch):07ad83db0fb67c5023bd627a61efb7f474c52622"

meta-fsl-demos    = "(nobranch):5a12677ad000a926d23c444266722a778ea228a7"

meta-fsl-arm     

meta-fsl-demos    = "(nobranch):d6764148c7cfea01b76f831671534a142e2eac2f"

NOTE: Preparing runqueue

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

WARNING: Failed to fetch URL ftp://ftp.ossp.org/pkg/lib/uuid/uuid-1.6.2.tar.gz, attempting MIRRORS if available

WARNING: Failed to fetch URL http://zlib.net/pigz/pigz-2.3.tar.gz, attempting MIRRORS if available

WARNING: Failed to fetch URL http://www.apache.org/dist/apr/apr-1.4.8.tar.bz2, attempting MIRRORS if available

WARNING: Failed to fetch URL http://www.apache.org/dist/apr/apr-util-1.5.2.tar.gz, attempting MIRRORS if available

WARNING: Failed to fetch URL http://www.apache.org/dist/subversion/subversion-1.7.10.tar.bz2, attempting MIRRORS if available

WARNING: Failed to fetch URL ftp://ftp.debian.org/debian/pool/main/n/netbase/netbase_5.1.tar.gz, attempting MIRRORS if available

WARNING: Failed to fetch URL ftp://ftp.debian.org/debian/pool/main/d/dpkg/dpkg_1.17.1.tar.xz, attempting MIRRORS if available

WARNING: Duplicate inclusion for /home/stephen.harper/fsl-community-bsp/sources/poky/meta/recipes-bsp/u-boot/u-boot.inc in /home/stephen.harper/fsl-community-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2013.04.bbappend

WARNING: Duplicate inclusion for /home/stephen.harper/fsl-community-bsp/sources/poky/meta/recipes-bsp/u-boot/u-boot.inc in /home/stephen.harper/fsl-community-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2013.04.bbappend

WARNING: Duplicate inclusion for /home/stephen.harper/fsl-community-bsp/sources/poky/meta/recipes-bsp/u-boot/u-boot.inc in /home/stephen.harper/fsl-community-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2013.04.bbappend

WARNING: Duplicate inclusion for /home/stephen.harper/fsl-community-bsp/sources/poky/meta/recipes-bsp/u-boot/u-boot.inc in /home/stephen.harper/fsl-community-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2013.04.bbappend

WARNING: Duplicate inclusion for /home/stephen.harper/fsl-community-bsp/sources/poky/meta/recipes-bsp/u-boot/u-boot.inc in /home/stephen.harper/fsl-community-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2013.04.bbappend

WARNING: Failed to fetch URL ftp://ftp.uni-erlangen.de/pub/Linux/LOCAL/dosfstools/dosfstools-2.11.src.tar.gz, attempting MIRRORS if available

WARNING: Duplicate inclusion for /home/stephen.harper/fsl-community-bsp/sources/poky/meta/recipes-bsp/u-boot/u-boot.inc in /home/stephen.harper/fsl-community-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2013.04.bbappend

WARNING: Duplicate inclusion for /home/stephen.harper/fsl-community-bsp/sources/poky/meta/recipes-bsp/u-boot/u-boot.inc in /home/stephen.harper/fsl-community-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2013.04.bbappend

WARNING: Duplicate inclusion for /home/stephen.harper/fsl-community-bsp/sources/poky/meta/recipes-bsp/u-boot/u-boot.inc in /home/stephen.harper/fsl-community-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2013.04.bbappend

WARNING: Duplicate inclusion for /home/stephen.harper/fsl-community-bsp/sources/poky/meta/recipes-bsp/u-boot/u-boot.inc in /home/stephen.harper/fsl-community-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2013.04.bbappend

WARNING: Duplicate inclusion for /home/stephen.harper/fsl-community-bsp/sources/poky/meta/recipes-bsp/u-boot/u-boot.inc in /home/stephen.harper/fsl-community-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2013.04.bbappend

WARNING: Duplicate inclusion for /home/stephen.harper/fsl-community-bsp/sources/poky/meta/recipes-bsp/u-boot/u-boot.inc in /home/stephen.harper/fsl-community-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2013.04.bbappend

WARNING: Duplicate inclusion for /home/stephen.harper/fsl-community-bsp/sources/poky/meta/recipes-bsp/u-boot/u-boot.inc in /home/stephen.harper/fsl-community-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx_2013.04.bbappend

ERROR: Function failed: do_rootfs (log file is located at /home/stephen.harper/fsl-community-bsp/build/tmp/work/imx6slevk-poky-linux-gnueabi/core-image-minimal/1.0-r0/temp/log.do_rootfs.1602)

ERROR: Logfile of failure stored in: /home/stephen.harper/fsl-community-bsp/build/tmp/work/imx6slevk-poky-linux-gnueabi/core-image-minimal/1.0-r0/temp/log.do_rootfs.1602

Log data follows:

| DEBUG: Executing python function rootfs_process_ignore

| DEBUG: Python function rootfs_process_ignore finished

| DEBUG: Executing python function rootfs_runtime_mapping

| DEBUG: Python function rootfs_runtime_mapping finished

| DEBUG: Executing shell function do_rootfs

| Previous repo file missing: /home/stephen.harper/fsl-community-bsp/build/tmp/deploy/rpm/all/repodata/primary.xml.gz

| Previous repo file missing: /home/stephen.harper/fsl-community-bsp/build/tmp/deploy/rpm/cortexa9hf_vfp_neon/repodata/primary.xml.gz

| Previous repo file missing: /home/stephen.harper/fsl-community-bsp/build/tmp/deploy/rpm/imx6slevk/repodata/primary.xml.gz

| Note: configuring RPM platform settings

| Note: configuring RPM system provides

| Note: configuring RPM DB settings

| Note: configuring Smart settings

|

|

|

|

|

|

| Note: adding Smart channel imx6slevk (65)

|

|

| Note: adding Smart channel cortexa9hf_vfp_neon (55)

|

|

| Note: adding Smart channel all (10)

|

|

| Note: configuring RPM cross-install scriptlet_wrapper

|

| Updating cache...               ######################################## [100%]

|

| Saving cache...

|

| Note: adding Smart RPM DB channel

|

| Note: to be installed:  run-postinsts@cortexa9hf_vfp_neon packagegroup-core-boot@imx6slevk

| Loading cache...

| Updating cache...               ######################################## [100%]

|

| Computing transaction...error: Can't install sysvinit-inittab-2.88dsf-r10@imx6slevk: no package provides /bin/bash

|

| Saving cache...

|

| WARNING: exit code 1 from a shell command.

| ERROR: Function failed: do_rootfs (log file is located at /home/stephen.harper/fsl-community-bsp/build/tmp/work/imx6slevk-poky-linux-gnueabi/core-image-minimal/1.0-r0/temp/log.do_rootfs.1602)

ERROR: Task 7 (/home/stephen.harper/fsl-community-bsp/sources/poky/meta/recipes-core/images/core-image-minimal.bb, do_rootfs) failed with exit code '1'

NOTE: Tasks Summary: Attempted 1606 tasks of which 261 didn't need to be rerun and 1 failed.

No currently running tasks (1606 of 1607)

Summary: 1 task failed:

  /home/stephen.harper/fsl-community-bsp/sources/poky/meta/recipes-core/images/core-image-minimal.bb, do_rootfs

Summary: There were 24 WARNING messages shown.

Summary: There was 1 ERROR message shown, returning a non-zero exit code.

Contents of the log file:

DEBUG: Executing python function rootfs_process_ignore

DEBUG: Python function rootfs_process_ignore finished

DEBUG: Executing python function rootfs_runtime_mapping

DEBUG: Python function rootfs_runtime_mapping finished

DEBUG: Executing shell function do_rootfs

Previous repo file missing: /home/stephen.harper/fsl-community-bsp/build/tmp/deploy/rpm/all/repodata/primary.xml.gz

Previous repo file missing: /home/stephen.harper/fsl-community-bsp/build/tmp/deploy/rpm/cortexa9hf_vfp_neon/repodata/primary.xml.gz

Previous repo file missing: /home/stephen.harper/fsl-community-bsp/build/tmp/deploy/rpm/imx6slevk/repodata/primary.xml.gz

Note: configuring RPM platform settings

Note: configuring RPM system provides

Note: configuring RPM DB settings

Note: configuring Smart settings

Note: adding Smart channel imx6slevk (65)

Note: adding Smart channel cortexa9hf_vfp_neon (55)

Note: adding Smart channel all (10)

Note: configuring RPM cross-install scriptlet_wrapper

Updating cache...               ######################################## [100%]

Saving cache...

Note: adding Smart RPM DB channel

Note: to be installed:  run-postinsts@cortexa9hf_vfp_neon packagegroup-core-boot@imx6slevk

Loading cache...

Updating cache...               ######################################## [100%]

Computing transaction...error: Can't install sysvinit-inittab-2.88dsf-r10@imx6slevk: no package provides /bin/bash

Saving cache...

WARNING: exit code 1 from a shell command.

ERROR: Function failed: do_rootfs (log file is located at /home/stephen.harper/fsl-community-bsp/build/tmp/work/imx6slevk-poky-linux-gnueabi/core-image-minimal/1.0-r0/temp/log.do_rootfs.1602)

0 件の賞賛
返信
8,826件の閲覧回数
LeonardoSandova
Specialist I

Stephen

Sorry, I did not pay attention to the manifest.xml step. You need to replace the original one with the one on the layer (not just adding the

meta-fsl-bsp-release.git - Freescale i.MX Yocto BSP Release Layer

This manifest is the one Freescale did full testing; as you can see, it is pointing to specific commits in time, no branches names. With the same build folder you have, just replace the manifest, sync & bake.

0 件の賞賛
返信
8,826件の閲覧回数
stephenharper
Contributor II

Gave that a shot. Again on a completely fresh environment, this time also including that step. Same result:

ERROR: Task 7 (/home/stephen.harper/fsl-community-bsp/sources/poky/meta/recipes-core/images/core-image-minimal.bb, do_rootfs) failed with exit code '1'

And the log file still contains:

Computing transaction...error: Can't install sysvinit-inittab-2.88dsf-r10@imx6slevk: no package provides /bin/bash

0 件の賞賛
返信
8,826件の閲覧回数
LeonardoSandova
Specialist I

Stephen, which host OS are you running bitbake? Please post this issue into the meta-freescale list, the list for meta-fsl-arm issues.

LaurenPost, have you run into this issue?

0 件の賞賛
返信
8,826件の閲覧回数
stephenharper
Contributor II

Leo, thanks again for your help. As I mentioned originally, I am running on Ubuntu 12.04

Perhaps I was a bit confused. Nowhere can I seem to locate fsl-yocto-release-manifest.xml as mentioned in the documentation.

Is the meta-fsl-bsp-release.git - Freescale i.MX Yocto BSP Release Layer manifest that you linked to above the one I should be using? (Because that's what I did)

0 件の賞賛
返信
8,826件の閲覧回数
LeonardoSandova
Specialist I

Yes, that is the manifest file to be used. Please post the question into the meta-freescale list. Although you are using non-community layers, people there can point to directions.

0 件の賞賛
返信
8,826件の閲覧回数
Rodrigue
NXP Employee
NXP Employee

Hi Leonardo, Even using the very same manifest I get it hanging at the same stage. I cleaned everything, resynchronised with the repository. I could not get rif of this issue either. As Stephen I am on a KUbuntu 12.04

0 件の賞賛
返信
8,826件の閲覧回数
Rodrigue
NXP Employee
NXP Employee

actually adding a bash dependency in the sysvinit-inittab_2.88dsf recipe fixed the issue. Just include RDEPENDS_${PN} += "bash" in the file.

8,826件の閲覧回数
stephenharper
Contributor II

This solved the build error and everything completes successfully and runs just fine. Thanks!

EDIT: (Update)

Just to clarify, adding the aforementioned RDEPENDS_${PN} += "bash" was in the recipe found at: /fsl-community-bsp/sources/poky/meta/recipes-core/sysvinit/sysvinit-inittab_2.88dsf.bb

(for me anyway)

find -name "sysvinit-inittab*" may prove useful to you if you do not have this exact path.

0 件の賞賛
返信
8,827件の閲覧回数
LeonardoSandova
Specialist I

Thanks Rodrigue. Seems like you got a patch to send to the OE list :smileyhappy:

0 件の賞賛
返信