Yocto Standard SDK vs Extensible SDK: What is the difference ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Yocto Standard SDK vs Extensible SDK: What is the difference ?

跳至解决方案
3,231 次查看
khang_letruong
Senior Contributor III

Dear Yocto Experts,

I learnt about Yocto Extensible SDK from following discussion : https://community.nxp.com/t5/i-MX-Processors/Yocto-Hardknott-and-iMX8MP-error-generating-extended-sd...

I would like to know what is the difference if any.

Thanks in advance and best regards,

Khang

0 项奖励
回复
1 解答
3,193 次查看
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

As per Yocto eSDK Manual:

The extensible SDK provides a cross-development toolchain and libraries tailored to the contents of a specific image. You would use the Extensible SDK if you want a toolchain experience supplemented with the powerful set of devtool commands tailored for the Yocto Project environment.

The installed extensible SDK consists of several files and directories. Basically, it contains an SDK environment setup script, some configuration files, an internal build system, and the devtool functionality.

As you can see in Yocto eSDK Manual and Toradex Community, devtool is the main feature of it.

Regards

在原帖中查看解决方案

0 项奖励
回复
1 回复
3,194 次查看
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

As per Yocto eSDK Manual:

The extensible SDK provides a cross-development toolchain and libraries tailored to the contents of a specific image. You would use the Extensible SDK if you want a toolchain experience supplemented with the powerful set of devtool commands tailored for the Yocto Project environment.

The installed extensible SDK consists of several files and directories. Basically, it contains an SDK environment setup script, some configuration files, an internal build system, and the devtool functionality.

As you can see in Yocto eSDK Manual and Toradex Community, devtool is the main feature of it.

Regards

0 项奖励
回复