I have not found anything real concrete on this. In LTIB there were settings in the menuconfig to be able to set a default IP address, subnet, etc... and turn the dhcp server off. The kernel uses the UDHCPC and gives the following while booting.
IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
udhcpc (v1.22.1) started
Sending discover...
Sending discover...
Sending discover...
No lease, forking to background
done.
I am not sure if this can be done from the machine conf file or if I need an .bbappend file somewhere.
Thanks
Michael
解決済! 解決策の投稿を見る。
 
					
				
		
I was able to include the updated interfaces file in yocto by doing the following so others can do this as well. I added recipes-core in my layer and then added an init-ifupdown folder. Inside that folder I added an init-ifupdown_1.0.bbappend file that contains only;
FILESEXTRAPATHS_prepend := "${THISDIR}/init-ifupdown-1.0:"
Then I put a init-ifupdown-1.0 folder that contains my updated interfaces file for yocto to include.
This is what my interfaces file contains where I set the eth0 to static and manually set it's address.
# /etc/network/interfaces -- configuration file for ifup(8), ifdown(8)
# The loopback interface
auto lo
iface lo inet loopback
# Wireless interfaces
iface wlan0 inet dhcp
wireless_mode managed
wireless_essid any
wpa-driver wext
wpa-conf /etc/wpa_supplicant.conf
iface atml0 inet dhcp
# Wired or wireless interfaces
auto eth0
iface eth0 inet static
address 10.254.253.1
netmask 255.255.255.0
iface eth1 inet dhcp
# Ethernet/RNDIS gadget (g_ether)
# ... or on host side, usbnet and random hwaddr
iface usb0 inet static
address 192.168.7.2
netmask 255.255.255.0
network 192.168.7.0
gateway 192.168.7.1
# Bluetooth networking
iface bnep0 inet dhcp
Hope this is helpful for someone else.
 
					
				
		
I was able to include the updated interfaces file in yocto by doing the following so others can do this as well. I added recipes-core in my layer and then added an init-ifupdown folder. Inside that folder I added an init-ifupdown_1.0.bbappend file that contains only;
FILESEXTRAPATHS_prepend := "${THISDIR}/init-ifupdown-1.0:"
Then I put a init-ifupdown-1.0 folder that contains my updated interfaces file for yocto to include.
This is what my interfaces file contains where I set the eth0 to static and manually set it's address.
# /etc/network/interfaces -- configuration file for ifup(8), ifdown(8)
# The loopback interface
auto lo
iface lo inet loopback
# Wireless interfaces
iface wlan0 inet dhcp
wireless_mode managed
wireless_essid any
wpa-driver wext
wpa-conf /etc/wpa_supplicant.conf
iface atml0 inet dhcp
# Wired or wireless interfaces
auto eth0
iface eth0 inet static
address 10.254.253.1
netmask 255.255.255.0
iface eth1 inet dhcp
# Ethernet/RNDIS gadget (g_ether)
# ... or on host side, usbnet and random hwaddr
iface usb0 inet static
address 192.168.7.2
netmask 255.255.255.0
network 192.168.7.0
gateway 192.168.7.1
# Bluetooth networking
iface bnep0 inet dhcp
Hope this is helpful for someone else.
Let me take up this question again. I have performed the steps that you indicate and the problem is when restarting the board does not assign static ip until it does not launch:
Ifdown eth0
Ifup eth0
Do you know what the problem may be?
Thank you.
i have the same behavior. i guess it do this because the actual default configuration is systemd. and init.d scripts are not executed.
 
					
				
		
This is really helpful. Thank you.
 
					
				
		
 Yuri
		
			Yuri
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		  The Yocto does not provide additional pseudo-graphical configuration tool, as
 the menuconfig for kernel, which was used under LTIB. 
 Looks like the only solution is to prepare proper file (manually), that should be located 
 in /etc/network/interfaces of rootfs.
Template is located in
<Yocto_dir>/fsl-release-bsp/sources/poky/meta-yocto-bsp/recipes-core/init-ifupdown
 Please use Linux command 
 
 $ man 5 interfaces 
 
 
for more details about file “interfaces”
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
 
					
				
		
Thank you for this information. I was able to adjust the interfaces file and that worked. Now I just need yocto to place the modified one in my image.