Yocto-SDK: populate_sdk failed on imx8qxpc0mek

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Yocto-SDK: populate_sdk failed on imx8qxpc0mek

2,619 次查看
wasim_nazir
Contributor II

Hi All,

Failing to run this command "DISTRO=fsl-imx-wayland MACHINE=imx8qxpc0mek bitbake imx-image-full -c populate_sdk" for imx-yocto-L4.14.78_1.0.0_ga:

I tried the following but still, it didn't work:
    2) Comment out the line: PACKAGE_CLASSES = "package_deb" conf/local.conf
 
Any lead will be appreciated.
 
Thanks In Advance
Wasim
 
 
0 项奖励
回复
2 回复数

2,605 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Can you attach the error log?

0 项奖励
回复

2,579 次查看
balaji1
Contributor II

Hi,

I tried the same using the command: bitbake imx-image-full -c populate_sdk

Thanks,

0 项奖励
回复