Yocto-SDK: populate_sdk failed on imx8qxpc0mek

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto-SDK: populate_sdk failed on imx8qxpc0mek

2,541件の閲覧回数
wasim_nazir
Contributor II

Hi All,

Failing to run this command "DISTRO=fsl-imx-wayland MACHINE=imx8qxpc0mek bitbake imx-image-full -c populate_sdk" for imx-yocto-L4.14.78_1.0.0_ga:

I tried the following but still, it didn't work:
    2) Comment out the line: PACKAGE_CLASSES = "package_deb" conf/local.conf
 
Any lead will be appreciated.
 
Thanks In Advance
Wasim
 
 
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,527件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Can you attach the error log?

0 件の賞賛
返信

2,501件の閲覧回数
balaji1
Contributor II

Hi,

I tried the same using the command: bitbake imx-image-full -c populate_sdk

Thanks,

0 件の賞賛
返信