Yocto-SDK: populate_sdk failed on imx8qxpc0mek

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto-SDK: populate_sdk failed on imx8qxpc0mek

2,470 Views
wasim_nazir
Contributor II

Hi All,

Failing to run this command "DISTRO=fsl-imx-wayland MACHINE=imx8qxpc0mek bitbake imx-image-full -c populate_sdk" for imx-yocto-L4.14.78_1.0.0_ga:

I tried the following but still, it didn't work:
    2) Comment out the line: PACKAGE_CLASSES = "package_deb" conf/local.conf
 
Any lead will be appreciated.
 
Thanks In Advance
Wasim
 
 
0 Kudos
Reply
2 Replies

2,456 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Can you attach the error log?

0 Kudos
Reply

2,430 Views
balaji1
Contributor II

Hi,

I tried the same using the command: bitbake imx-image-full -c populate_sdk

Thanks,

0 Kudos
Reply