Yocto Project build error imx8m mini

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Yocto Project build error imx8m mini

2,038 次查看
inigovicentewal
Contributor III

Hi,

I'm trying to build yocto project ZEUS for imx8m mini.

I have this configuration EXTRA_IMAGE_FEATURES= “ ssh-server-openssh tools-sdk tools-debug dbg-pkgs dev-pkgs doc-pkgs package-management tools-profile” in my build/conf/local.con file.

But it reports error when executing bitbake core-image-base.
Host environment: Ubuntu 18.04.3 LTS

Can any one explain how to resolve this?

The error log is below:

bitbake core-image-base

Loading cache: 100% |################################################################################################| Time: 0:00:04

Loaded 3447 entries from dependency cache.

NOTE: Resolving any missing task queue dependencies

 

Build Configuration:

BB_VERSION           = "1.44.0"

BUILD_SYS            = "x86_64-linux"

NATIVELSBSTRING      = "universal"

TARGET_SYS           = "aarch64-fslc-linux"

MACHINE              = "imx8mmevk"

DISTRO               = "fslc-xwayland"

DISTRO_VERSION       = "3.0"

TUNE_FEATURES        = "aarch64 cortexa53 crc crypto"

TARGET_FPU           = ""

meta                

meta-poky            = "HEAD:c204cc47d0a319d0435c4a9ba06e241c2e75ff1e"

meta-oe             

meta-multimedia     

meta-python          = "HEAD:bb65c27a772723dfe2c15b5e1b27bcc1a1ed884c"

meta-freescale       = "HEAD:3a3b13bef12c3a46da976fbf3b666310f8b694a7"

meta-freescale-3rdparty = "HEAD:aea3771baa77e74762358ceb673d407e36637e5f"

meta-freescale-distro = "HEAD:ca27d12e4964d1336e662bcc60184bbff526c857"

 

Initialising tasks: 100% |###########################################################################################| Time: 0:00:12

Sstate summary: Wanted 1034 Found 0 Missed 1034 Current 764 (0% match, 42% complete)

NOTE: Executing Tasks

NOTE: Setscene tasks completed

ERROR: perf-1.0-r9 do_compile: oe_runmake failed

ERROR: perf-1.0-r9 do_compile: Execution of '/home/iv/imx/fsl-community-bsp/build/tmp/work/imx8mmevk-fslc-linux/perf/1.0-r9/temp/run.do_compile.8170' failed with exit code 1:

make: Entering directory '/home/iv/imx/fsl-community-bsp/build/tmp/work/imx8mmevk-fslc-linux/perf/1.0-r9/perf-1.0/tools/perf'

  BUILD:   Doing 'make -j1' parallel build

Warning: Kernel ABI header at 'tools/include/uapi/drm/drm.h' differs from latest version at 'include/uapi/drm/drm.h'

Warning: Kernel ABI header at 'tools/include/uapi/linux/kvm.h' differs from latest version at 'include/uapi/linux/kvm.h'

Warning: Kernel ABI header at 'tools/arch/x86/include/asm/disabled-features.h' differs from latest version at 'arch/x86/include/asm/disabled-features.h'

Warning: Kernel ABI header at 'tools/arch/x86/include/asm/required-features.h' differs from latest version at 'arch/x86/include/asm/required-features.h'

Warning: Kernel ABI header at 'tools/arch/x86/include/asm/cpufeatures.h' differs from latest version at 'arch/x86/include/asm/cpufeatures.h'

Warning: Kernel ABI header at 'tools/arch/arm/include/uapi/asm/perf_regs.h' differs from latest version at 'arch/arm/include/uapi/asm/perf_regs.h'

Warning: Kernel ABI header at 'tools/arch/arm64/include/uapi/asm/perf_regs.h' differs from latest version at 'arch/arm64/include/uapi/asm/perf_regs.h'

Warning: Kernel ABI header at 'tools/arch/powerpc/include/uapi/asm/perf_regs.h' differs from latest version at 'arch/powerpc/include/uapi/asm/perf_regs.h'

Warning: Kernel ABI header at 'tools/arch/x86/include/uapi/asm/perf_regs.h' differs from latest version at 'arch/x86/include/uapi/asm/perf_regs.h'

Warning: Kernel ABI header at 'tools/arch/x86/include/uapi/asm/kvm.h' differs from latest version at 'arch/x86/include/uapi/asm/kvm.h'

Warning: Kernel ABI header at 'tools/arch/x86/include/uapi/asm/kvm_perf.h' differs from latest version at 'arch/x86/include/uapi/asm/kvm_perf.h'

Warning: Kernel ABI header at 'tools/arch/x86/include/uapi/asm/svm.h' differs from latest version at 'arch/x86/include/uapi/asm/svm.h'

Warning: Kernel ABI header at 'tools/arch/x86/include/uapi/asm/unistd.h' differs from latest version at 'arch/x86/include/uapi/asm/unistd.h'

Warning: Kernel ABI header at 'tools/arch/x86/include/uapi/asm/vmx.h' differs from latest version at 'arch/x86/include/uapi/asm/vmx.h'

Warning: Kernel ABI header at 'tools/arch/powerpc/include/uapi/asm/kvm.h' differs from latest version at 'arch/powerpc/include/uapi/asm/kvm.h'

Warning: Kernel ABI header at 'tools/arch/s390/include/uapi/asm/kvm.h' differs from latest version at 'arch/s390/include/uapi/asm/kvm.h'

Warning: Kernel ABI header at 'tools/arch/s390/include/uapi/asm/kvm_perf.h' differs from latest version at 'arch/s390/include/uapi/asm/kvm_perf.h'

Warning: Kernel ABI header at 'tools/arch/s390/include/uapi/asm/sie.h' differs from latest version at 'arch/s390/include/uapi/asm/sie.h'

Warning: Kernel ABI header at 'tools/arch/arm/include/uapi/asm/kvm.h' differs from latest version at 'arch/arm/include/uapi/asm/kvm.h'

Warning: Kernel ABI header at 'tools/arch/arm64/include/uapi/asm/kvm.h' differs from latest version at 'arch/arm64/include/uapi/asm/kvm.h'

Warning: Kernel ABI header at 'tools/arch/x86/lib/memcpy_64.S' differs from latest version at 'arch/x86/lib/memcpy_64.S'

Warning: Kernel ABI header at 'tools/arch/x86/lib/memset_64.S' differs from latest version at 'arch/x86/lib/memset_64.S'

 

Auto-detecting system features:

...                         dwarf: [ on  ]

...            dwarf_getlocations: [ on  ]

...                         glibc: [ on  ]

...                          gtk2: [ OFF ]

...                      libaudit: [ OFF ]

...                        libbfd: [ on  ]

...                        libelf: [ on  ]

...                       libnuma: [ OFF ]

...        numa_num_possible_cpus: [ OFF ]

...                       libperl: [ OFF ]

...                     libpython: [ on  ]

...                      libslang: [ on  ]

...                     libcrypto: [ on  ]

...                     libunwind: [ on  ]

...            libdw-dwarf-unwind: [ on  ]

...                          zlib: [ on  ]

...                          lzma: [ on  ]

...                     get_cpuid: [ OFF ]

...                           bpf: [ on  ]

 

Makefile.config:391: DWARF support is off, BPF prologue is disabled

Makefile.config:588: Missing perl devel files. Disabling perl scripting support, please install perl-ExtUtils-Embed/libperl-dev

Makefile.config:626: Python 3 is not yet supported; please set

Makefile.config:627: PYTHON and/or PYTHON_CONFIG appropriately.

Makefile.config:628: If you also have Python 2 installed, then

Makefile.config:629: try something like:

Makefile.config:630:

Makefile.config:631:   make PYTHON=python2

Makefile.config:632:

Makefile.config:633: Otherwise, disable Python support entirely:

Makefile.config:634:

Makefile.config:635:   make NO_LIBPYTHON=1

Makefile.config:636:

Makefile.config:637: *** .  Stop.

Makefile.perf:203: recipe for target 'sub-make' failed

make[1]: *** [sub-make] Error 2

Makefile:69: recipe for target 'all' failed

make: *** [all] Error 2

make: Leaving directory '/home/iv/imx/fsl-community-bsp/build/tmp/work/imx8mmevk-fslc-linux/perf/1.0-r9/perf-1.0/tools/perf'

WARNING: exit code 1 from a shell command.

 

ERROR: Logfile of failure stored in: /home/iv/imx/fsl-community-bsp/build/tmp/work/imx8mmevk-fslc-linux/perf/1.0-r9/temp/log.do_compile.8170

Log data follows:

| DEBUG: Executing shell function do_compile

| NOTE: make -j 1 -C /home/iv/imx/fsl-community-bsp/build/tmp/work/imx8mmevk-fslc-linux/perf/1.0-r9/perf-1.0/tools/perf O=/home/iv/imx/fsl-community-bsp/build/tmp/work/imx8mmevk-fslc-linux/perf/1.0-r9/perf-1.0 CROSS_COMPILE=aarch64-fslc-linux- ARCH=arm64 CC=aarch64-fslc-linux-gcc  -mcpu=cortex-a53+crc+crypto -fstack-protector-strong  -D_FORTIFY_SOURCE=2 -Wformat -Wformat-security -Werror=format-security -O2 -pipe -g -feliminate-unused-debug-types -fmacro-prefix-map=/home/iv/imx/fsl-community-bsp/build/tmp/work/imx8mmevk-fslc-linux/perf/1.0-r9=/usr/src/debug/perf/1.0-r9                      -fdebug-prefix-map=/home/iv/imx/fsl-community-bsp/build/tmp/work/imx8mmevk-fslc-linux/perf/1.0-r9=/usr/src/debug/perf/1.0-r9                      -fdebug-prefix-map=/home/iv/imx/fsl-community-bsp/build/tmp/work/imx8mmevk-fslc-linux/perf/1.0-r9/recipe-sysroot=                      -fdebug-prefix-map=/home/iv/imx/fsl-community-bsp/build/tmp/work/imx8mmevk-fslc-linux/perf/1.0-r9/recipe-sysroot-native=  --sysroot=/home/iv/imx/fsl-community-bsp/build/tmp/work/imx8mmevk-fslc-linux/perf/1.0-r9/recipe-sysroot AR=aarch64-fslc-linux-gcc-ar LD=aarch64-fslc-linux-ld --sysroot=/home/iv/imx/fsl-community-bsp/build/tmp/work/imx8mmevk-fslc-linux/perf/1.0-r9/recipe-sysroot  EXTRA_CFLAGS=-ldw EXTRA_LDFLAGS= perfexecdir=/usr/libexec NO_GTK2=1 NO_LIBAUDIT=1 NO_DWARF=1 NO_JVMTI=1 NO_LIBNUMA=1 NO_SDT=1 TMPDIR=/home/iv/imx/fsl-community-bsp/build/tmp/work/imx8mmevk-fslc-linux/perf/1.0-r9/perf-1.0 LIBUNWIND_DIR=/home/iv/imx/fsl-community-bsp/build/tmp/work/imx8mmevk-fslc-linux/perf/1.0-r9/recipe-sysroot/usr DESTDIR=/home/iv/imx/fsl-community-bsp/build/tmp/work/imx8mmevk-fslc-linux/perf/1.0-r9/image prefix=/usr bindir=/usr/bin sharedir=/usr/share sysconfdir=/etc perfexecdir=/usr/libexec/perf-core ETC_PERFCONFIG=../etc sharedir=share mandir=share/man infodir=share/info PYTHON=python3 PYTHON_CONFIG=python3-config all

| make: Entering directory '/home/iv/imx/fsl-community-bsp/build/tmp/work/imx8mmevk-fslc-linux/perf/1.0-r9/perf-1.0/tools/perf'

|   BUILD:   Doing 'make -j1' parallel build

| Warning: Kernel ABI header at 'tools/include/uapi/drm/drm.h' differs from latest version at 'include/uapi/drm/drm.h'

| Warning: Kernel ABI header at 'tools/include/uapi/linux/kvm.h' differs from latest version at 'include/uapi/linux/kvm.h'

| Warning: Kernel ABI header at 'tools/arch/x86/include/asm/disabled-features.h' differs from latest version at 'arch/x86/include/asm/disabled-features.h'

| Warning: Kernel ABI header at 'tools/arch/x86/include/asm/required-features.h' differs from latest version at 'arch/x86/include/asm/required-features.h'

| Warning: Kernel ABI header at 'tools/arch/x86/include/asm/cpufeatures.h' differs from latest version at 'arch/x86/include/asm/cpufeatures.h'

| Warning: Kernel ABI header at 'tools/arch/arm/include/uapi/asm/perf_regs.h' differs from latest version at 'arch/arm/include/uapi/asm/perf_regs.h'

| Warning: Kernel ABI header at 'tools/arch/arm64/include/uapi/asm/perf_regs.h' differs from latest version at 'arch/arm64/include/uapi/asm/perf_regs.h'

| Warning: Kernel ABI header at 'tools/arch/powerpc/include/uapi/asm/perf_regs.h' differs from latest version at 'arch/powerpc/include/uapi/asm/perf_regs.h'

| Warning: Kernel ABI header at 'tools/arch/x86/include/uapi/asm/perf_regs.h' differs from latest version at 'arch/x86/include/uapi/asm/perf_regs.h'

| Warning: Kernel ABI header at 'tools/arch/x86/include/uapi/asm/kvm.h' differs from latest version at 'arch/x86/include/uapi/asm/kvm.h'

| Warning: Kernel ABI header at 'tools/arch/x86/include/uapi/asm/kvm_perf.h' differs from latest version at 'arch/x86/include/uapi/asm/kvm_perf.h'

| Warning: Kernel ABI header at 'tools/arch/x86/include/uapi/asm/svm.h' differs from latest version at 'arch/x86/include/uapi/asm/svm.h'

| Warning: Kernel ABI header at 'tools/arch/x86/include/uapi/asm/unistd.h' differs from latest version at 'arch/x86/include/uapi/asm/unistd.h'

| Warning: Kernel ABI header at 'tools/arch/x86/include/uapi/asm/vmx.h' differs from latest version at 'arch/x86/include/uapi/asm/vmx.h'

| Warning: Kernel ABI header at 'tools/arch/powerpc/include/uapi/asm/kvm.h' differs from latest version at 'arch/powerpc/include/uapi/asm/kvm.h'

| Warning: Kernel ABI header at 'tools/arch/s390/include/uapi/asm/kvm.h' differs from latest version at 'arch/s390/include/uapi/asm/kvm.h'

| Warning: Kernel ABI header at 'tools/arch/s390/include/uapi/asm/kvm_perf.h' differs from latest version at 'arch/s390/include/uapi/asm/kvm_perf.h'

| Warning: Kernel ABI header at 'tools/arch/s390/include/uapi/asm/sie.h' differs from latest version at 'arch/s390/include/uapi/asm/sie.h'

| Warning: Kernel ABI header at 'tools/arch/arm/include/uapi/asm/kvm.h' differs from latest version at 'arch/arm/include/uapi/asm/kvm.h'

| Warning: Kernel ABI header at 'tools/arch/arm64/include/uapi/asm/kvm.h' differs from latest version at 'arch/arm64/include/uapi/asm/kvm.h'

| Warning: Kernel ABI header at 'tools/arch/x86/lib/memcpy_64.S' differs from latest version at 'arch/x86/lib/memcpy_64.S'

| Warning: Kernel ABI header at 'tools/arch/x86/lib/memset_64.S' differs from latest version at 'arch/x86/lib/memset_64.S'

|

| Auto-detecting system features:

| ...                         dwarf: [ on  ]

| ...            dwarf_getlocations: [ on  ]

| ...                         glibc: [ on  ]

| ...                          gtk2: [ OFF ]

| ...                      libaudit: [ OFF ]

| ...                        libbfd: [ on  ]

| ...                        libelf: [ on  ]

| ...                       libnuma: [ OFF ]

| ...        numa_num_possible_cpus: [ OFF ]

| ...                       libperl: [ OFF ]

| ...                     libpython: [ on  ]

| ...                      libslang: [ on  ]

| ...                     libcrypto: [ on  ]

| ...                     libunwind: [ on  ]

| ...            libdw-dwarf-unwind: [ on  ]

| ...                          zlib: [ on  ]

| ...                          lzma: [ on  ]

| ...                     get_cpuid: [ OFF ]

| ...                           bpf: [ on  ]

|

| Makefile.config:391: DWARF support is off, BPF prologue is disabled

| Makefile.config:588: Missing perl devel files. Disabling perl scripting support, please install perl-ExtUtils-Embed/libperl-dev

| Makefile.config:626: Python 3 is not yet supported; please set

| Makefile.config:627: PYTHON and/or PYTHON_CONFIG appropriately.

| Makefile.config:628: If you also have Python 2 installed, then

| Makefile.config:629: try something like:

| Makefile.config:630:

| Makefile.config:631:   make PYTHON=python2

| Makefile.config:632:

| Makefile.config:633: Otherwise, disable Python support entirely:

| Makefile.config:634:

| Makefile.config:635:   make NO_LIBPYTHON=1

| Makefile.config:636:

| Makefile.config:637: *** .  Stop.

| Makefile.perf:203: recipe for target 'sub-make' failed

| make[1]: *** [sub-make] Error 2

| ERROR: oe_runmake failed

| Makefile:69: recipe for target 'all' failed

| make: *** [all] Error 2

| make: Leaving directory '/home/iv/imx/fsl-community-bsp/build/tmp/work/imx8mmevk-fslc-linux/perf/1.0-r9/perf-1.0/tools/perf'

| WARNING: exit code 1 from a shell command.

| ERROR: Execution of '/home/iv/imx/fsl-community-bsp/build/tmp/work/imx8mmevk-fslc-linux/perf/1.0-r9/temp/run.do_compile.8170' failed with exit code 1:

| make: Entering directory '/home/iv/imx/fsl-community-bsp/build/tmp/work/imx8mmevk-fslc-linux/perf/1.0-r9/perf-1.0/tools/perf'

|   BUILD:   Doing 'make -j1' parallel build

| Warning: Kernel ABI header at 'tools/include/uapi/drm/drm.h' differs from latest version at 'include/uapi/drm/drm.h'

| Warning: Kernel ABI header at 'tools/include/uapi/linux/kvm.h' differs from latest version at 'include/uapi/linux/kvm.h'

| Warning: Kernel ABI header at 'tools/arch/x86/include/asm/disabled-features.h' differs from latest version at 'arch/x86/include/asm/disabled-features.h'

| Warning: Kernel ABI header at 'tools/arch/x86/include/asm/required-features.h' differs from latest version at 'arch/x86/include/asm/required-features.h'

| Warning: Kernel ABI header at 'tools/arch/x86/include/asm/cpufeatures.h' differs from latest version at 'arch/x86/include/asm/cpufeatures.h'

| Warning: Kernel ABI header at 'tools/arch/arm/include/uapi/asm/perf_regs.h' differs from latest version at 'arch/arm/include/uapi/asm/perf_regs.h'

| Warning: Kernel ABI header at 'tools/arch/arm64/include/uapi/asm/perf_regs.h' differs from latest version at 'arch/arm64/include/uapi/asm/perf_regs.h'

| Warning: Kernel ABI header at 'tools/arch/powerpc/include/uapi/asm/perf_regs.h' differs from latest version at 'arch/powerpc/include/uapi/asm/perf_regs.h'

| Warning: Kernel ABI header at 'tools/arch/x86/include/uapi/asm/perf_regs.h' differs from latest version at 'arch/x86/include/uapi/asm/perf_regs.h'

| Warning: Kernel ABI header at 'tools/arch/x86/include/uapi/asm/kvm.h' differs from latest version at 'arch/x86/include/uapi/asm/kvm.h'

| Warning: Kernel ABI header at 'tools/arch/x86/include/uapi/asm/kvm_perf.h' differs from latest version at 'arch/x86/include/uapi/asm/kvm_perf.h'

| Warning: Kernel ABI header at 'tools/arch/x86/include/uapi/asm/svm.h' differs from latest version at 'arch/x86/include/uapi/asm/svm.h'

| Warning: Kernel ABI header at 'tools/arch/x86/include/uapi/asm/unistd.h' differs from latest version at 'arch/x86/include/uapi/asm/unistd.h'

| Warning: Kernel ABI header at 'tools/arch/x86/include/uapi/asm/vmx.h' differs from latest version at 'arch/x86/include/uapi/asm/vmx.h'

| Warning: Kernel ABI header at 'tools/arch/powerpc/include/uapi/asm/kvm.h' differs from latest version at 'arch/powerpc/include/uapi/asm/kvm.h'

| Warning: Kernel ABI header at 'tools/arch/s390/include/uapi/asm/kvm.h' differs from latest version at 'arch/s390/include/uapi/asm/kvm.h'

| Warning: Kernel ABI header at 'tools/arch/s390/include/uapi/asm/kvm_perf.h' differs from latest version at 'arch/s390/include/uapi/asm/kvm_perf.h'

| Warning: Kernel ABI header at 'tools/arch/s390/include/uapi/asm/sie.h' differs from latest version at 'arch/s390/include/uapi/asm/sie.h'

| Warning: Kernel ABI header at 'tools/arch/arm/include/uapi/asm/kvm.h' differs from latest version at 'arch/arm/include/uapi/asm/kvm.h'

| Warning: Kernel ABI header at 'tools/arch/arm64/include/uapi/asm/kvm.h' differs from latest version at 'arch/arm64/include/uapi/asm/kvm.h'

| Warning: Kernel ABI header at 'tools/arch/x86/lib/memcpy_64.S' differs from latest version at 'arch/x86/lib/memcpy_64.S'

| Warning: Kernel ABI header at 'tools/arch/x86/lib/memset_64.S' differs from latest version at 'arch/x86/lib/memset_64.S'

|

| Auto-detecting system features:

| ...                         dwarf: [ on  ]

| ...            dwarf_getlocations: [ on  ]

| ...                         glibc: [ on  ]

| ...                          gtk2: [ OFF ]

| ...                      libaudit: [ OFF ]

| ...                        libbfd: [ on  ]

| ...                        libelf: [ on  ]

| ...                       libnuma: [ OFF ]

| ...        numa_num_possible_cpus: [ OFF ]

| ...                       libperl: [ OFF ]

| ...                     libpython: [ on  ]

| ...                      libslang: [ on  ]

| ...                     libcrypto: [ on  ]

| ...                     libunwind: [ on  ]

| ...            libdw-dwarf-unwind: [ on  ]

| ...                          zlib: [ on  ]

| ...                          lzma: [ on  ]

| ...                     get_cpuid: [ OFF ]

| ...                           bpf: [ on  ]

|

| Makefile.config:391: DWARF support is off, BPF prologue is disabled

| Makefile.config:588: Missing perl devel files. Disabling perl scripting support, please install perl-ExtUtils-Embed/libperl-dev

| Makefile.config:626: Python 3 is not yet supported; please set

| Makefile.config:627: PYTHON and/or PYTHON_CONFIG appropriately.

| Makefile.config:628: If you also have Python 2 installed, then

| Makefile.config:629: try something like:

| Makefile.config:630:

| Makefile.config:631:   make PYTHON=python2

| Makefile.config:632:

| Makefile.config:633: Otherwise, disable Python support entirely:

| Makefile.config:634:

| Makefile.config:635:   make NO_LIBPYTHON=1

| Makefile.config:636:

| Makefile.config:637: *** .  Stop.

| Makefile.perf:203: recipe for target 'sub-make' failed

| make[1]: *** [sub-make] Error 2

| Makefile:69: recipe for target 'all' failed

| make: *** [all] Error 2

| make: Leaving directory '/home/iv/imx/fsl-community-bsp/build/tmp/work/imx8mmevk-fslc-linux/perf/1.0-r9/perf-1.0/tools/perf'

| WARNING: exit code 1 from a shell command.

|

ERROR: Task (/home/iv/imx/fsl-community-bsp/sources/poky/meta/recipes-kernel/perf/perf.bb:do_compile) failed with exit code '1'

NOTE: Tasks Summary: Attempted 3272 tasks of which 3269 didn't need to be rerun and 1 failed.

NOTE: Writing buildhistory

NOTE: Writing buildhistory took: 10 seconds

 

Summary: 1 task failed:

  /home/iv/imx/fsl-community-bsp/sources/poky/meta/recipes-kernel/perf/perf.bb:do_compile

Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

THANKS!

标签 (1)
0 项奖励
回复
1 回复

1,805 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Iñigo Vicente,

Are you using the Community BSP?

I would recommend against using the Zeus branch for now. It is a bit early in its development and while it’s stable, there may still be some work to be one. I would recommend Sumo or Thud if you are using the Community BSP.

This does not mean that the error may not present itself, but changes of encountering errors should be minimal. I also would suggest that you first bake the image as is, and then add additional packages, to isolate what could be the problem.


Regards,

0 项奖励
回复