Yocto Project Build Error on i.MX6q Saberauto

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Yocto Project Build Error on i.MX6q Saberauto

2,049 次查看
351814019
Contributor I

Hi,

I'm trying to build yocto project for imx6q saberauto according to 《i.MX_YOCYO_Project_User's_Guide.pdf》.

But it reports error when executing bitbake fsl-image-gui .
Host environment: Ubuntu-14.04.

Can any one explain how to resolve this?

The error log is below:


yocto@ubuntu:/work/fsl-release-bsp/imx6qsabresd$ bitbake fsl-image-gui
NOTE: Your conf/bblayers.conf has been automatically updated.
Parsing recipes: 100% |#########################################| Time: 00:02:25
Parsing of 2215 .bb files complete (0 cached, 2215 parsed). 2790 targets, 434 skipped, 5 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.30.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-14.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6qsabresd"
DISTRO = "fsl-imx-fb"
DISTRO_VERSION = "4.1.15-2.1.0"
TUNE_FEATURES = "arm armv7a vfp neon callconvention-hard cortexa9"
TARGET_FPU = "hard"
meta
meta-yocto = "HEAD:f5da2a5913319ad6ac2141438ba1aa17576326ab"
meta-oe
meta-multimedia = "HEAD:247b1267bbe95719cd4877d2d3cfbaf2a2f4865a"
meta-fsl-arm = "HEAD:be78894e4682f111575470fb23e51e6ba523508d"
meta-fsl-arm-extra = "HEAD:3dfb82fc7e703eae9891b3ffda0e9393701f2396"
meta-fsl-demos = "HEAD:a165068f8a0d1cf29aabe4b4053f28be1c2aa492"
meta-bsp
meta-sdk = "HEAD:823b26a67261270d2bf22d511e6190641a8a90cf"
meta-browser = "HEAD:77736988073a5d90fcff9d0005c8477332ede387"
meta-gnome
meta-networking
meta-python
meta-filesystems = "HEAD:247b1267bbe95719cd4877d2d3cfbaf2a2f4865a"
meta-qt5 = "HEAD:ccae79be69c5268df3b47e4e14cea0591c39a531"

NOTE: Preparing RunQueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: cpuburn-neon-20140626-r0 do_fetch: Unable to acquire lock '/work/fsl-release-bsp/downloads//cpuburn-neon-20140626/burn.S.lock', directory is not writable
ERROR: cpuburn-neon-20140626-r0 do_fetch: Function failed: base_do_fetch
ERROR: Logfile of failure stored in: /work/fsl-release-bsp/imx6qsabresd/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/cpuburn-neon/20140626-r0/temp/log.do_fetch.42915
ERROR: Task 2615 (/work/fsl-release-bsp/sources/meta-openembedded/meta-oe/recipes-benchmark/cpuburn/cpuburn-neon_20140626.bb, do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 1494 tasks of which 0 didn't need to be rerun and 1 failed.
Waiting for 0 running tasks to finish:

Summary: 1 task failed:
/work/fsl-release-bsp/sources/meta-openembedded/meta-oe/recipes-benchmark/cpuburn/cpuburn-neon_20140626.bb, do_fetch
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

标签 (1)
0 项奖励
回复
3 回复数

1,798 次查看
karangajjar
Senior Contributor II

Hi 文博 尚,

Please verify below two things:

1. No other process is using the work directory. (May be some other Yocto compilation is midway)

2. You have write permission for the work directory.

Regards,

Karan Gajjar

0 项奖励
回复

1,798 次查看
351814019
Contributor I

Thank you very much!!!

0 项奖励
回复

1,798 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Good!!!

0 项奖励
回复