Yocto NXP GA release and meta-freescale mismatch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto NXP GA release and meta-freescale mismatch

Jump to solution
346 Views
securemetersczhang
Contributor II

Hi, I am working on upgrading Linux for an old HW platform using i.MX6UL.

I am trying to freeze a version/tag/commit for the Yocto meta-imx and meta-freescale.

But I found version mismatch when I refer to GA release when bitbake firmware-imx.

I have put all the detailed steps and logs in README in this repo.
scarthgap-6.6.23-2.0.0 
scarthgap-6.6.36-2.1.0 

Please follow these two branches to re-produce the problem described in the "Known issue" section:
scarthgap-6.6.23-2.0.0 known-issue 
scarthgap-6.6.36-2.1.0 known-issue 

Please help to look at this issue. Thanks in advance!

BR/Chencheng

Labels (2)
0 Kudos
Reply
1 Solution
168 Views
securemetersczhang
Contributor II

Hi Chavira,

I bumped all the meta layers to use imx GA 6.6.52 2.2.0 release.

And this particular issue is gone.

BR/Chencheng

View solution in original post

0 Kudos
Reply
2 Replies
324 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @securemetersczhang!

Thank you for contacting NXP Support!

 

Unfortunately we can't do nothing since is not an official repo.

Please download the source code from the official NXP repository.

 

Best Regards!

Chavira

0 Kudos
Reply
169 Views
securemetersczhang
Contributor II

Hi Chavira,

I bumped all the meta layers to use imx GA 6.6.52 2.2.0 release.

And this particular issue is gone.

BR/Chencheng

0 Kudos
Reply