Hi, I am working on upgrading Linux for an old HW platform using i.MX6UL.
I am trying to freeze a version/tag/commit for the Yocto meta-imx and meta-freescale.
But I found version mismatch when I refer to GA release when bitbake firmware-imx.
I have put all the detailed steps and logs in README in this repo.
scarthgap-6.6.23-2.0.0
scarthgap-6.6.36-2.1.0
Please follow these two branches to re-produce the problem described in the "Known issue" section:
scarthgap-6.6.23-2.0.0 known-issue
scarthgap-6.6.36-2.1.0 known-issue
Please help to look at this issue. Thanks in advance!
BR/Chencheng
Solved! Go to Solution.
Hi Chavira,
I bumped all the meta layers to use imx GA 6.6.52 2.2.0 release.
And this particular issue is gone.
BR/Chencheng
Thank you for contacting NXP Support!
Unfortunately we can't do nothing since is not an official repo.
Please download the source code from the official NXP repository.
Best Regards!
Chavira
Hi Chavira,
I bumped all the meta layers to use imx GA 6.6.52 2.2.0 release.
And this particular issue is gone.
BR/Chencheng