Yocto Hardknott and iMX8MP: error generating extended sdk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto Hardknott and iMX8MP: error generating extended sdk

Jump to solution
3,790 Views
pierluigi_p
Senior Contributor I

Dear NXP team,

when running the command

    bitbake fsl-image-qt5 -c populate_sdk_ext

the file /usr/bin/protoc is provided by both protobuf-native and tensorflow-protobuf-native, aborting the build.

Assuming (from the history of the current recipe) that protobuf and tensorflow-protobuf should cohexist, I suppose than protoc could be renamed to tf-protoc in tensorflow-protobuf recipe.

Could you please double check the attached patch and possibly integrate in meta-imx ?

Thanks

Best Regards

Pier

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
3,749 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

I can see the same issue and i will post your patch in next bsp test.

View solution in original post

0 Kudos
Reply
4 Replies
3,754 Views
pierluigi_p
Senior Contributor I

The problem is reproducible running

    bitbake imx-image-full -c populate_sdk_ext

Can't you ?

Thanks

Best Regards

Pier

3,750 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

I can see the same issue and i will post your patch in next bsp test.

0 Kudos
Reply
3,725 Views
pierluigi_p
Senior Contributor I

Thanks!

Best Regards

Pier

0 Kudos
Reply
3,767 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

I didn't make fsl-image-qt5 in hardkott before,but our support images are imx-image-full、imx-image-multimedia

0 Kudos
Reply