Yocto(Dora) build with kernel 3.10.9-alpha for imx6q-sabreauto kernel panic

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto(Dora) build with kernel 3.10.9-alpha for imx6q-sabreauto kernel panic

2,105 Views
seongjoondoh
Contributor I

I tried to build image for imx6q-sabreauto with kernel 3.10.9-alpha.

It seem to be running into a few problems.

I am using a manifest.xml from meta-fsl-bsp-release.git - Freescale i.MX Yocto BSP Release Layer.

I got a new image without no build error. However, I met kernel panic after starting kernel.

(I have successfully run the image from kernel 3.0.35 using same microSD card.)

=====================================================================

U-Boot 2013.04 (Feb 07 2014 - 17:21:47)

CPU:   Freescale i.MX6Q rev1.2 at 792 MHz

CPU:   Temperature 32 C, calibration data: 0x5664b87d

Reset cause: POR

Board: MX6Q/SDL-Sabreauto revA

I2C:   ready

DRAM:  2 GiB

NAND:  No NAND device found!!!

0 MiB

MMC:   FSL_SDHC: 0

*** Warning - bad CRC, using default environment

In:    serial

Out:   serial

Err:   serial

Found PFUZE100! deviceid=10,revid=11

Net:   FEC [PRIME]

Warning: FEC using MAC address from net device

Hit any key to stop autoboot:  0

mmc0 is current device

reading boot.scr

** Unable to read file boot.scr **

reading uImage

5237688 bytes read in 247 ms (20.2 MiB/s)

Booting from mmc ...

reading imx6q-sabreauto.dtb

44626 bytes read in 19 ms (2.2 MiB/s)

## Booting kernel from Legacy Image at 12000000 ...

   Image Name:   Linux-3.10.9-1.0.0_alpha+d

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    5237624 Bytes = 5 MiB

   Load Address: 10008000

   Entry Point:  10008000

   Verifying Checksum ... OK

## Flattened Device Tree blob at 18000000

   Booting using the fdt blob at 0x18000000

   Loading Kernel Image ... OK

OK

   Using Device Tree in place at 18000000, end 1800de51

Starting kernel ...

Booting Linux on physical CPU 0x0

...............

mmc0: no vqmmc regulator found

mmc0: no vmmc regulator found

mmc0: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA

ata1: SATA link down (SStatus 0 SControl 300)

mmc0: Problem setting current limit!

mmc0: new ultra high speed DDR50 SDHC card at address aaaa

mmcblk0: mmc0:aaaa SU32G 29.7 GiB

mmcblk0: error -84 transferring data, sector 0, nr 8, cmd response 0x900, card status 0xb00

mmcblk0: retrying using single block read

mmcblk0: error -84 transferring data, sector 0, nr 8, cmd response 0x900, card status 0x0

end_request: I/O error, dev mmcblk0, sector 0

mmc0: Got data interrupt 0x00000002 even though no data operation was in progress.

mmcblk0: error -84 transferring data, sector 1, nr 7, cmd response 0x900, card status 0x0

end_request: I/O error, dev mmcblk0, sector 1

mmc0: Got data interrupt 0x00000002 even though no data operation was in progress.

mmcblk0: error -84 transferring data, sector 2, nr 6, cmd response 0x900, card status 0x0

end_request: I/O error, dev mmcblk0, sector 2

mmc0: Got data interrupt 0x00000002 even though no data operation was in progress.

mmcblk0: error -84 transferring data, sector 3, nr 5, cmd response 0x900, card status 0x0

end_request: I/O error, dev mmcblk0, sector 3

mmcblk0: error -84 transferring data, sector 4, nr 4, cmd response 0x900, card status 0x0

end_request: I/O error, dev mmcblk0, sector 4

mmcblk0: error -84 transferring data, sector 5, nr 3, cmd response 0x900, card status 0x0

end_request: I/O error, dev mmcblk0, sector 5

mmcblk0: error -84 transferring data, sector 6, nr 2, cmd response 0x900, card status 0x0

end_request: I/O error, dev mmcblk0, sector 6

mmcblk0: error -84 transferring data, sector 7, nr 1, cmd response 0x900, card status 0x0

end_request: I/O error, dev mmcblk0, sector 7

Buffer I/O error on device mmcblk0, logical block 0

mmcblk0: error -84 transferring data, sector 0, nr 8, cmd response 0x900, card status 0xb00

mmcblk0: retrying using single block read

mmcblk0: error -84 transferring data, sector 0, nr 8, cmd response 0x900, card status 0x0

end_request: I/O error, dev mmcblk0, sector 0

mmcblk0: error -84 transferring data, sector 1, nr 7, cmd response 0x900, card status 0x0

end_request: I/O error, dev mmcblk0, sector 1

mmcblk0: error -84 transferring data, sector 2, nr 6, cmd response 0x900, card status 0x0

mmcblk0: error -84 transferring data, sector 3, nr 5, cmd response 0x900, card status 0x0

mmc0: Got data interrupt 0x00000002 even though no data operation was in progress.

mmcblk0: error -84 transferring data, sector 4, nr 4, cmd response 0x900, card status 0x0

mmcblk0: error -84 transferring data, sector 5, nr 3, cmd response 0x900, card status 0x0

mmc0: Got data interrupt 0x00000002 even though no data operation was in progress.

mmcblk0: error -84 transferring data, sector 6, nr 2, cmd response 0x900, card status 0x0

mmc0: Got data interrupt 0x00000002 even though no data operation was in progress.

mmcblk0: error -84 transferring data, sector 7, nr 1, cmd response 0x900, card status 0x0

Buffer I/O error on device mmcblk0, logical block 0

mmcblk0: error -84 transferring data, sector 0, nr 8, cmd response 0x900, card status 0xb00

mmcblk0: retrying using single block read

mmcblk0: error -84 transferring data, sector 0, nr 8, cmd response 0x900, card status 0x0

mmcblk0: error -84 transferring data, sector 1, nr 7, cmd response 0x900, card status 0x0

mmc0: Got data interrupt 0x00000002 even though no data operation was in progress.

mmcblk0: error -84 transferring data, sector 2, nr 6, cmd response 0x900, card status 0x0

mmcblk0: error -84 transferring data, sector 3, nr 5, cmd response 0x900, card status 0x0

mmcblk0: error -84 transferring data, sector 4, nr 4, cmd response 0x900, card status 0x0

mmcblk0: error -84 transferring data, sector 5, nr 3, cmd response 0x900, card status 0x0

mmcblk0: error -84 transferring data, sector 6, nr 2, cmd response 0x900, card status 0x0

mmc0: Got data interrupt 0x00000002 even though no data operation was in progress.

mmcblk0: error -84 transferring data, sector 7, nr 1, cmd response 0x900, card status 0x0

Buffer I/O error on device mmcblk0, logical block 0

mmcblk0: unable to read partition table

...........

...........

platform sound-fm.32: Driver imx-tuner-si476x requests probe deferral

ALSA device list:

  #0: cs42888-audio

  #1: imx-spdif

  #2: imx-hdmi-soc

VFS: Cannot open root device "mmcblk0p2" or unknown-block(179,2): error -6

Please append a correct "root=" boot option; here are the available partitions:

b300        31166976 mmcblk0  driver: mmcblk

Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2)

.......

0 Kudos
Reply
3 Replies

1,387 Views
YixingKong
Senior Contributor IV

Seongjoon

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

0 Kudos
Reply

1,387 Views
YixingKong
Senior Contributor IV

Seongjoon

We have not got your response yet and will close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply

1,387 Views
YixingKong
Senior Contributor IV

Seongjoon

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply