Hi,
I am trying to generate core-image-base for imx8mmevk board. What is the yocto DISTRO configuration needs to be used imx8mmevk board ?
The below part in the Yocto Project Users guide is confusing. Is it referring to i.MX8 only or i.MX8M also ?
• fsl-imx-x11 - X11 graphics are not supported on i.MX 8.
• fsl-imx-wayland - Wayland weston graphics.
• fsl-imx-xwayland - Wayland graphics and X11. X11 applications using EGL are not supported.
• fsl-imx-fb - Frame Buffer graphics - no X11 or Wayland. Frame Buffer is not supported on i.MX 8.
Thanks for your help in advance,
Regards,
Vijay.
I have tested fsl-imx-xwayland, and bitbake fsl-image-validation-imx successfully, you can use fsl-imx-wayland too
Thanks Joan Xie !!!.