Hi NXP,
I create patches for the kernel (linux-imx_5.15.bbappend), but the kernel versions are shown to be: Linux version 5.15.71
FILESEXTRAPATHS:prepend := "${THISDIR}/${PN}:"
SRC_URI += "file://0001-my-released.patch"
KERNEL_VERSION_SANITY_SKIP="1"
KERNEL_DEBUG_TIMESTAMPS = "1"
SCMVERSION = "n"
The meta-imx/recipes-kernel/linux/linux-imx_5.15.bb has the option:
LOCALVERSION = "-lts-next"So I guess the correct kernel version should be: Linux version 5.15.71-lts-next
And I check linux-imx/5.15.71+gitAUTOINC+d286e47181-r0/build/.config
The content inside is always:
CONFIG_LOCALVERSION=""
CONFIG_LOCALVERSION_AUTO=y
I tried adding the patch from
https://github.com/Freescale/meta-freescale/commit/e5401e6aebbc15617b4397db6cb5fa103db144bc
However, the display of the kernel version has not changed.
Regards,
解決済! 解決策の投稿を見る。
Hi Joanxie,
I have switched to using the LF6.1.22-2.0.0 imx manifest.
This issue has been resolved.
Regards,
what result do you need and what you get indeed? pls share more detailed information, pls share the log you get, let me double check it
Hi Joanxie,
I have switched to using the LF6.1.22-2.0.0 imx manifest.
This issue has been resolved.
Regards,