Hi NXP,
I create patches for the kernel (linux-imx_5.15.bbappend), but the kernel versions are shown to be: Linux version 5.15.71
FILESEXTRAPATHS:prepend := "${THISDIR}/${PN}:"
SRC_URI += "file://0001-my-released.patch"
KERNEL_VERSION_SANITY_SKIP="1"
KERNEL_DEBUG_TIMESTAMPS = "1"
SCMVERSION = "n"
The meta-imx/recipes-kernel/linux/linux-imx_5.15.bb has the option:
LOCALVERSION = "-lts-next"So I guess the correct kernel version should be: Linux version 5.15.71-lts-next
And I check linux-imx/5.15.71+gitAUTOINC+d286e47181-r0/build/.config
The content inside is always:
CONFIG_LOCALVERSION=""
CONFIG_LOCALVERSION_AUTO=y
I tried adding the patch from
https://github.com/Freescale/meta-freescale/commit/e5401e6aebbc15617b4397db6cb5fa103db144bc
However, the display of the kernel version has not changed.
Regards,
已解决! 转到解答。
Hi Joanxie,
I have switched to using the LF6.1.22-2.0.0 imx manifest.
This issue has been resolved.
Regards,