Yocto Build imx.6 Qt5 Build Error due to Ubuntu 18.04 System headers

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Yocto Build imx.6 Qt5 Build Error due to Ubuntu 18.04 System headers

跳至解决方案
3,965 次查看
alptugcalik
Contributor I

I have setup the Yocto Project and built successfully a Linux image for my board. It works properly for simple applications. However, for some of my applications , the toolchain crashes. The header files in the toolchain tries to reach the headers in my ubuntu 18.04 system files. How can i solve this?

My qmake.conf file:

MAKEFILE_GENERATOR = UNIX
CONFIG += incremental
QMAKE_INCREMENTAL_STYLE = sublib
QMAKE_PLATFORM += linux unix posix
QMAKE_LEX = flex
QMAKE_LEXFLAGS +=
QMAKE_YACC = yacc
QMAKE_YACCFLAGS += -d
QMAKE_YACCFLAGS_MANGLE += -p $base -b $base
QMAKE_YACC_HEADER = $base.tab.h
QMAKE_YACC_SOURCE = $base.tab.c
QMAKE_PREFIX_SHLIB = lib
QMAKE_EXTENSION_SHLIB = so
QMAKE_PREFIX_STATICLIB = lib
QMAKE_EXTENSION_STATICLIB = a
QMAKE_CFLAGS_THREAD += -D_REENTRANT
QMAKE_CXXFLAGS_THREAD += $$QMAKE_CFLAGS_THREAD
QMAKE_LFLAGS_GCSECTIONS = -Wl,--gc-sections
QMAKE_LFLAGS_REL_RPATH = -Wl,-z,origin
QMAKE_REL_RPATH_BASE = $ORIGIN
QMAKE_INCDIR =
QMAKE_LIBDIR =
QMAKE_INCDIR_X11 =
QMAKE_LIBDIR_X11 =
QMAKE_INCDIR_OPENGL =
QMAKE_LIBDIR_OPENGL =
QMAKE_INCDIR_OPENGL_ES2 = $$QMAKE_INCDIR_OPENGL
QMAKE_LIBDIR_OPENGL_ES2 = $$QMAKE_LIBDIR_OPENGL
QMAKE_INCDIR_EGL =
QMAKE_LIBDIR_EGL =
QMAKE_INCDIR_OPENVG =
QMAKE_LIBDIR_OPENVG =
QMAKE_LIBS =
QMAKE_LIBS_DYNLOAD = -ldl
QMAKE_LIBS_X11 = -lXext -lX11 -lm
QMAKE_LIBS_NIS = -lnsl
QMAKE_LIBS_EGL = -lEGL
QMAKE_LIBS_OPENGL = -lGL
QMAKE_LIBS_OPENGL_ES2 = -lGLESv2
QMAKE_LIBS_OPENVG = -lOpenVG
QMAKE_LIBS_THREAD = -lpthread
QMAKE_LIBS_LIBUDEV = -ludev
QMAKE_CFLAGS_WAYLAND =
QMAKE_INCDIR_WAYLAND =
QMAKE_LIBS_WAYLAND_CLIENT = -lwayland-client
QMAKE_LIBS_WAYLAND_SERVER = -lwayland-server
QMAKE_LIBDIR_WAYLAND =
QMAKE_DEFINES_WAYLAND =
QMAKE_WAYLAND_SCANNER = wayland-scanner
QMAKE_CFLAGS_XCB =
QMAKE_LIBS_XCB =
QMAKE_DEFINES_XCB =
QMAKE_AR = arm-poky-linux-gnueabi-ar cqs
QMAKE_OBJCOPY = arm-poky-linux-gnueabi-objcopy
QMAKE_NM = arm-poky-linux-gnueabi-nm -P
QMAKE_RANLIB = arm-poky-linux-gnueabi-ranlib
QMAKE_STRIP = arm-poky-linux-gnueabi-strip
QMAKE_STRIPFLAGS_LIB += --strip-unneeded
QMAKE_CFLAGS_OPTIMIZE = -O2
QMAKE_CFLAGS_OPTIMIZE_FULL = -O3
QMAKE_CFLAGS += -pipe
QMAKE_CFLAGS_DEPS += -M
QMAKE_CFLAGS_WARN_ON += -Wall -W
QMAKE_CFLAGS_WARN_OFF += -w
QMAKE_CFLAGS_RELEASE += $$QMAKE_CFLAGS_OPTIMIZE
QMAKE_CFLAGS_RELEASE_WITH_DEBUGINFO += $$QMAKE_CFLAGS_OPTIMIZE -g
QMAKE_CFLAGS_DEBUG += -g -feliminate-unused-debug-types
QMAKE_CFLAGS_SHLIB += -fPIC
QMAKE_CFLAGS_STATIC_LIB += -fPIC
QMAKE_CFLAGS_APP += -fPIC
QMAKE_CFLAGS_ISYSTEM = -isystem
QMAKE_CFLAGS_YACC += -Wno-unused -Wno-parentheses
QMAKE_CFLAGS_HIDESYMS += -fvisibility=hidden
QMAKE_CFLAGS_EXCEPTIONS_OFF += -fno-exceptions
QMAKE_CFLAGS_SPLIT_SECTIONS += -ffunction-sections
QMAKE_CFLAGS_LTCG = -flto -fno-fat-lto-objects
QMAKE_CFLAGS_LTCG_FATOBJECTS = -ffat-lto-objects
QMAKE_CFLAGS_DISABLE_LTCG = -fno-lto
QMAKE_CFLAGS_SSE2 += -msse2
QMAKE_CFLAGS_SSE3 += -msse3
QMAKE_CFLAGS_SSSE3 += -mssse3
QMAKE_CFLAGS_SSE4_1 += -msse4.1
QMAKE_CFLAGS_SSE4_2 += -msse4.2
QMAKE_CFLAGS_AVX += -mavx
QMAKE_CFLAGS_AVX2 += -mavx2
QMAKE_CFLAGS_NEON += -mfpu=neon
QMAKE_CFLAGS_PRECOMPILE = -x c-header -c ${QMAKE_PCH_INPUT} -o ${QMAKE_PCH_OUTPUT}
QMAKE_CFLAGS_USE_PRECOMPILE = -include ${QMAKE_PCH_OUTPUT_BASE}
QMAKE_CXXFLAGS += $$QMAKE_CFLAGS
QMAKE_CXXFLAGS_DEPS += $$QMAKE_CFLAGS_DEPS
QMAKE_CXXFLAGS_WARN_ON += $$QMAKE_CFLAGS_WARN_ON
QMAKE_CXXFLAGS_WARN_OFF += $$QMAKE_CFLAGS_WARN_OFF
QMAKE_CXXFLAGS_RELEASE += $$QMAKE_CFLAGS_RELEASE
QMAKE_CXXFLAGS_RELEASE_WITH_DEBUGINFO += $$QMAKE_CFLAGS_RELEASE_WITH_DEBUGINFO
QMAKE_CXXFLAGS_DEBUG += $$QMAKE_CFLAGS_DEBUG
QMAKE_CXXFLAGS_SHLIB += $$QMAKE_CFLAGS_SHLIB
QMAKE_CXXFLAGS_STATIC_LIB += $$QMAKE_CFLAGS_STATIC_LIB
QMAKE_CXXFLAGS_APP += $$QMAKE_CFLAGS_APP
QMAKE_CXXFLAGS_YACC += $$QMAKE_CFLAGS_YACC
QMAKE_CXXFLAGS_HIDESYMS += $$QMAKE_CFLAGS_HIDESYMS -fvisibility-inlines-hidden
QMAKE_CXXFLAGS_EXCEPTIONS_OFF += $$QMAKE_CFLAGS_EXCEPTIONS_OFF
QMAKE_CXXFLAGS_SPLIT_SECTIONS += $$QMAKE_CFLAGS_SPLIT_SECTIONS
QMAKE_CXXFLAGS_LTCG = $$QMAKE_CFLAGS_LTCG
QMAKE_CXXFLAGS_LTCG_FATOBJECTS = $$QMAKE_CFLAGS_LTCG_FATOBJECTS
QMAKE_CXXFLAGS_DISABLE_LTCG = $$QMAKE_CFLAGS_DISABLE_LTCG
QMAKE_CXXFLAGS_PRECOMPILE = -x c++-header -c ${QMAKE_PCH_INPUT} -o ${QMAKE_PCH_OUTPUT}
QMAKE_CXXFLAGS_USE_PRECOMPILE = $$QMAKE_CFLAGS_USE_PRECOMPILE
QMAKE_CXXFLAGS_CXX11 = -std=c++0x
QMAKE_CXXFLAGS_CXX14 = -std=c++1y
QMAKE_CXXFLAGS_CXX1Z = -std=c++1z
QMAKE_CXXFLAGS_GNUCXX11 = -std=gnu++0x
QMAKE_CXXFLAGS_GNUCXX14 = -std=gnu++1y
QMAKE_CXXFLAGS_GNUCXX1Z = -std=gnu++1z
QMAKE_LFLAGS += -Wl,--hash-style=gnu -Wl,--as-needed
QMAKE_LFLAGS_DEBUG +=
QMAKE_LFLAGS_APP +=
QMAKE_LFLAGS_RELEASE +=
QMAKE_LFLAGS_RELEASE_WITH_DEBUGINFO +=
QMAKE_LFLAGS_EXCEPTIONS_OFF +=
QMAKE_LFLAGS_LTCG = $$QMAKE_CFLAGS_LTCG -fuse-linker-plugin
QMAKE_LFLAGS_SHLIB += -shared
QMAKE_LFLAGS_PLUGIN += $$QMAKE_LFLAGS_SHLIB
QMAKE_LFLAGS_SONAME += -Wl,-soname,
QMAKE_LFLAGS_THREAD +=
QMAKE_LFLAGS_RPATH = -Wl,-rpath,
QMAKE_LFLAGS_RPATHLINK = -Wl,-rpath-link,
QMAKE_LFLAGS_NEW_DTAGS = -Wl,--enable-new-dtags
QMAKE_LFLAGS_USE_GOLD = -fuse-ld=gold
QMAKE_LFLAGS_BSYMBOLIC_FUNC = -Wl,-Bsymbolic-functions
QMAKE_LFLAGS_DYNAMIC_LIST = -Wl,--dynamic-list,
QMAKE_LFLAGS_VERSION_SCRIPT = -Wl,--version-script,
QMAKE_LFLAGS_CXX11 =
QMAKE_LFLAGS_CXX14 =
QMAKE_LFLAGS_CXX1Z =
QMAKE_LFLAGS_RELEASE += -Wl,-O1
QMAKE_LFLAGS_NOUNDEF += -Wl,--no-undefined
QMAKE_AR_LTCG = gcc-ar cqs
QMAKE_NM_LTCG = gcc-nm -P
QMAKE_RANLIB_LTCG = true # No need to run since gcc-ar has "s"
QMAKE_COMMON_SANITIZE_CFLAGS = -fno-omit-frame-pointer
QMAKE_COMMON_SANITIZE_CXXFLAGS = -fno-omit-frame-pointer
QMAKE_SANITIZE_ADDRESS_CFLAGS = -fsanitize=address
QMAKE_SANITIZE_ADDRESS_CXXFLAGS = -fsanitize=address
QMAKE_SANITIZE_ADDRESS_LFLAGS = -fsanitize=address
QMAKE_SANITIZE_THREAD_CFLAGS = -fsanitize=thread
QMAKE_SANITIZE_THREAD_CXXFLAGS = -fsanitize=thread
QMAKE_SANITIZE_THREAD_LFLAGS = -fsanitize=thread
QMAKE_SANITIZE_MEMORY_CFLAGS = -fsanitize=memory
QMAKE_SANITIZE_MEMORY_CXXFLAGS = -fsanitize=memory
QMAKE_SANITIZE_MEMORY_LFLAGS = -fsanitize=memory
QMAKE_SANITIZE_UNDEFINED_CFLAGS = -fsanitize=undefined
QMAKE_SANITIZE_UNDEFINED_CXXFLAGS = -fsanitize=undefined
QMAKE_SANITIZE_UNDEFINED_LFLAGS = -fsanitize=undefined
QMAKE_COMPILER = arm-poky-linux-gnueabi-gcc -march=armv7-a -mfpu=neon -mfloat-abi=hard -mcpu=cortex-a9 --sysroot=/opt/meta-toolchain-qt5/fsl-imx-xwayland/5.4-zeus/sysroots/cortexa9t2hf-neon-poky-linux-gnueabi
QMAKE_CC = arm-poky-linux-gnueabi-gcc -march=armv7-a -mfpu=neon -mfloat-abi=hard -mcpu=cortex-a9 --sysroot=/opt/meta-toolchain-qt5/fsl-imx-xwayland/5.4-zeus/sysroots/cortexa9t2hf-neon-poky-linux-gnueabi
QMAKE_LINK_C = $$QMAKE_CC
QMAKE_LINK_C_SHLIB = $$QMAKE_CC
QMAKE_CXX = arm-poky-linux-gnueabi-g++ -march=armv7-a -mfpu=neon -mfloat-abi=hard -mcpu=cortex-a9 --sysroot=/opt/meta-toolchain-qt5/fsl-imx-xwayland/5.4-zeus/sysroots/cortexa9t2hf-neon-poky-linux-gnueabi
QMAKE_LINK = $$QMAKE_CXX
QMAKE_LINK_SHLIB = $$QMAKE_CXX
QMAKE_PCH_OUTPUT_EXT = .gch
load(qt_config)

 

标签 (1)
0 项奖励
回复
1 解答
3,926 次查看
alptugcalik
Contributor I

Hello,

Thanks for your reply. I have found out that a variable IMX_SYSROOT is used in some of the project files in Qt5. By adding this variable to project environment variables, i solved the problem. I specifically point the directory where I build the SDK of the imx6 board.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,927 次查看
alptugcalik
Contributor I

Hello,

Thanks for your reply. I have found out that a variable IMX_SYSROOT is used in some of the project files in Qt5. By adding this variable to project environment variables, i solved the problem. I specifically point the directory where I build the SDK of the imx6 board.

0 项奖励
回复
3,934 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Alptugcalik,

How the application is crashing? the yocto run fine? then you have an issue with the application that is not supported by yocto.

Regards

 

0 项奖励
回复