Yocto Build Error for i.MX8M Plus with L5.4.70

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto Build Error for i.MX8M Plus with L5.4.70

Jump to solution
3,063 Views
Harrison_Choi
NXP Employee
NXP Employee

Hello Team

 

I am FAE to support Korean customer

I failed to build yocto for i.MX8M Plus with L5.4.70 as following the instruction in the following link

https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf

 

ERROR: kernel-module-isp-vvcam-4.2.2.6.0-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; unset _PYTHON_SYSCONFIGDATA_NAME; export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/1007/bus"; export PATH="/home/harrison/iMX_GA/imx-yocto-bsp-L5.4.70/sources/poky/scripts:/home/harrison/iMX_GA/imx-yocto-bsp-L5.4.70/build-8mp-xwayland/tmp/work/imx8mpevk-poky-linux/kernel-module-isp-vvcam/4.2.2.6.0-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux:/home/harrison/iMX_GA/imx-yocto-bsp-L5.4.70/build-8mp-xwayland/tmp/work/imx8mpevk-poky-linux/kernel-module-isp-vvcam/4.2.2.6.0-r0/recipe-sysroot/usr/bin/crossscripts:/home/harrison/iMX_GA/imx-yocto-bsp-L5.4.70/build-8mp-xwayland/tmp/work/imx8mpevk-poky-linux/kernel-module-isp-vvcam/4.2.2.6.0-r0/recipe-sysroot-native/usr/sbin:/home/harrison/iMX_GA/imx-yocto-bsp-L5.4.70/build-8mp-xwayland/tmp/work/imx8mpevk-poky-linux/kernel-module-isp-vvcam/4.2.2.6.0-r0/recipe-sysroot-native/usr/bin:/home/harrison/iMX_GA/imx-yocto-bsp-L5.4.70/build-8mp-xwayland/tmp/work/imx8mpevk-poky-linux/kernel-module-isp-vvcam/4.2.2.6.0-r0/recipe-sysroot-native/sbin:/home/harrison/iMX_GA/imx-yocto-bsp-L5.4.70/build-8mp-xwayland/tmp/work/imx8mpevk-poky-linux/kernel-module-isp-vvcam/4.2.2.6.0-r0/recipe-sysroot-native/bin:/home/harrison/iMX_GA/imx-yocto-bsp-L5.4.70/sources/poky/bitbake/bin:/home/harrison/iMX_GA/imx-yocto-bsp-L5.4.70/build-8mp-xwayland/tmp/hosttools"; export HOME="/home/harrison"; git -c core.fsyncobjectfiles=0 remote rm origin failed with exit code 1, output:

Note: Some branches outside the refs/remotes/ hierarchy were not removed;

to delete them, use:

  git branch -d imx_5.4.24_2.1.0

  git branch -d imx_5.4.47_2.2.0

error: could not lock config file config

error: Could not remove config section 'remote.origin'

 

ERROR: kernel-module-isp-vvcam-4.2.2.6.0-r0 do_fetch: Fetcher failure for URL: 'git://source.codeaurora.org/external/imx/isp-vvcam.git;protocol=https;branch=imx_5.4.70_2.3.0'. Unable to fetch URL from any source.

ERROR: Logfile of failure stored in: /home/harrison/iMX_GA/imx-yocto-bsp-L5.4.70/build-8mp-xwayland/tmp/work/imx8mpevk-poky-linux/kernel-module-isp-vvcam/4.2.2.6.0-r0/temp/log.do_fetch.24300

ERROR: Task (/home/harrison/iMX_GA/imx-yocto-bsp-L5.4.70/sources/meta-imx/meta-bsp/recipes-kernel/kernel-modules/kernel-module-isp-vvcam_4.2.2.6.0.bb:do_fetch) failed with exit code '1'

NOTE: Tasks Summary: Attempted 2317 tasks of which 2283 didn't need to be rerun and 1 failed.

 

Summary: 1 task failed:

  /home/harrison/iMX_GA/imx-yocto-bsp-L5.4.70/sources/meta-imx/meta-bsp/recipes-kernel/kernel-modules/kernel-module-isp-vvcam_4.2.2.6.0.bb:do_fetch

 

For reference, I have succeeded in building yocto for i.MX8M Mini/Nano and i.MX8QXP

 

Thanks

Harrison

0 Kudos
Reply
1 Solution
3,042 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the error message, it seems that your network issue, pls try to use the commands as below, and bitbake again

bitbake -c cleansstate  kernel-module-isp-vvcam

bitbake kernel-module-isp-vvcam

 

View solution in original post

0 Kudos
Reply
2 Replies
3,043 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the error message, it seems that your network issue, pls try to use the commands as below, and bitbake again

bitbake -c cleansstate  kernel-module-isp-vvcam

bitbake kernel-module-isp-vvcam

 

0 Kudos
Reply
3,037 Views
Harrison_Choi
NXP Employee
NXP Employee

Hello 

 

Thank you for your reply
As you said, there seems to be unknown problem in the network in build server that I am using

 

I will close this ticket

 

Thanks

Harrison

0 Kudos
Reply