[Yocto BSP 1.8] i.MX6DP Display issue on LVDS dual channel panel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[Yocto BSP 1.8] i.MX6DP Display issue on LVDS dual channel panel

1,831 次查看
charleshuang
Senior Contributor II

u-boot setting:

setenv mmcargs setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot} ${bootargs} video=mxcfb0:dev=ldb,if=RGB24 fbmem=24M

 

LVDS dual channel setting in dts file:

&ldb {

  status = "okay";

};

 

&mxcfb1 {

  status = "okay";

};

 

&mxcfb2 {

  disp_dev = "ldb";

  mode_str ="1280x1024M@60";

  status = "okay";

};

 

&mxcfb3 {

  disp_dev = "ldb";

  mode_str ="1280x1024M@60";

  status = "okay";

};

 

&ldb {

  ext_ref = "true";

  status = "okay";

  split-mode;

 

  lvds-channel@0 {

  fsl,data-mapping = "spwg";

  fsl,data-width = <24>;

  crtc = "ipu2-di0";

  primary;

  status = "okay";

 

  display-timings {

                        native-mode = <&timing0>;

                        timing0: g190eg01v1 {

                                clock-frequency = <54000000>;

                                hactive = <640>;

                                vactive = <1024>;

                                hback-porch = <108>;

                                hfront-porch = <40>;

                                vback-porch = <3>;

                                vfront-porch = <29>;

                                hsync-len = <68>;

                                vsync-len = <7>;

                        };

                };

  };

 

  lvds-channel@1 {

                fsl,data-mapping = "spwg";

                fsl,data-width = <24>;

                crtc = "ipu1-di1";

                status = "okay";

 

  display-timings {

                        native-mode = <&timing1>;

                        timing1: g190eg01v1 {

                                clock-frequency = <54000000>;

                                hactive = <640>;

                                vactive = <1024>;

                                hback-porch = <108>;

                                hfront-porch = <40>;

                                vback-porch = <3>;

                                vfront-porch = <29>;

                                hsync-len = <68>;

                                vsync-len = <7>;

                        };

                };

  };

};

 

When the device display QT window on LVDS dual channel panel (1280*1024 resolution), the quality of the image is very poor.

Please see attached file.

Can you tell me how to modify dts file?

 

Thank you.

Original Attachment has been moved to: lvds_pictures.zip

0 项奖励
回复
4 回复数

1,015 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Which BSP version are you using?

Are you trying to get an extended desktop or just clone the desktop?

Best Regards,

Alejandro

0 项奖励
回复

1,015 次查看
charleshuang
Senior Contributor II

Hi alejandrolozano,

I use BSP version is 3.14.52.

No. I just want to display QT desktop on a dual channel of lvds panel.

Thanks.

Best Regards,

Alex

0 项奖励
回复

1,015 次查看
强王
Contributor IV
this is my dts config:
  lvds_display: fb@0 {

        compatible = "fsl,mxc_sdc_fb";

        disp_dev = "ldb";

        interface_pix_fmt = "RGB24";

        mode_str ="LDB-XGA";

        default_bpp = <32>;

        int_clk = <0>;

        late_init = <0>;

        status = "okay";

    };

&ldb {

    status = "okay";

    split-mode;

    lvds-channel@0 {

        reg = <0>;

        crtc = "ipu2-di0";

        fsl,data-mapping = "spwg";

        fsl,data-width = <24>;

        status = "okay";

        display-timings {

            native-mode = <&timing0>;

            timing0: g104xvn01 {

                clock-frequency = <130000000>;

                hactive = <1920>;

                vactive = <720>;

                hback-porch = <40>;

                hfront-porch = <40>;

                vback-porch = <15>;

                vfront-porch = <15>;

                hsync-len = <80>;

                vsync-len = <10>;

            };

        };

    };

    lvds-channel@1 {

        reg = <1>;

        crtc = "ipu2-di1";

        fsl,data-mapping = "spwg";

        fsl,data-width = <24>;

        status = "okay";

        primary;

        display-timings {

            native-mode = <&timing1>;

            timing1: g104xvn01 {

                clock-frequency = <130000000>;

                hactive = <1920>;

                vactive = <720>;

                hback-porch = <40>;

                hfront-porch = <40>;

                vback-porch = <15>;

                vfront-porch = <15>;

                hsync-len = <80>;

                vsync-len = <10>;                                                                                                                            

            };

        };

    };

};

0 项奖励
回复

1,015 次查看
charleshuang
Senior Contributor II

I try your method, it also cannot work. It works fine on i.MX6. But this issue is occurred  on i.MX6DP.

Can you tell me how to solve this issue on i.MX6DP?

Thanks.

0 项奖励
回复