Yocto 5.0 kernel 6.6.23 Yocto compiler fail in imx8mp.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto 5.0 kernel 6.6.23 Yocto compiler fail in imx8mp.

Jump to solution
3,211 Views
charleshuang
Senior Contributor II

Hi NXP

Follow nxp github readme.  Yocto 5.0 kernel 6.6.23 Yocto compiler fail in imx8mp.

https://github.com/nxp-imx/imx-manifest/tree/imx-linux-scarthgap

MACHINE=imx8mp-lpddr4-evk DISTRO=fsl-imx-xwayland source ./imx-setup-release.sh -b imx8mp-lpddr4-evk

bitbake imx-image-full

Do you have any advice?

charleshuang_0-1719546537258.png

 

0 Kudos
Reply
1 Solution
3,128 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

What is the Ubuntu version are you using? It is the host machine configure root for the compile failed, in our side, we do not met the issue.

image (18).pngimage (17).png

Here recommend you to check and install all the Yocto Project host packages in the IMX_YOCTO_PROJECT_USERS_GUIDE

View solution in original post

0 Kudos
Reply
5 Replies
3,189 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You can refer to the document we released, if question still tell us.

Any questions contact us freely

0 Kudos
Reply
3,151 Views
charleshuang
Senior Contributor II

Hello @Rita_Wang 

I got the other Error shark "nnshark_2023.11.imx.bb:do_configure failed ...."

charleshuang_0-1719804409476.png

Since the Yocto 3.3, we and our customer always get the fail message about nnshark.

Please provide the nnshark on downloads for Yocto 5.0.

Thanks.

 

charleshuang_1-1719804641282.png

 

 

 

0 Kudos
Reply
3,129 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

What is the Ubuntu version are you using? It is the host machine configure root for the compile failed, in our side, we do not met the issue.

image (18).pngimage (17).png

Here recommend you to check and install all the Yocto Project host packages in the IMX_YOCTO_PROJECT_USERS_GUIDE

0 Kudos
Reply
3,109 Views
charleshuang
Senior Contributor II

Hi  @Rita_Wang 

Our ubuntu is 20.04, we user the docker.

We have solutions about fixed the nnshark fail issue.

Thanks for your help.

3,105 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi @charleshuang

Good news it works, could you share the method to us, so that met the some issue ones can refer to it. Great thanks.

Wish you have a nice day

Best Regards

Rita

0 Kudos
Reply