Dear Otavio,
Thanks your helpful answer before.
I would change test splash image feature.
According to Yocto BSP guide below, need to create a .bbappend.
Q1: Which folder need to place the .bbappend? sources/meta-fsl-arm, sources/poky/meta-yocto
Either or know bitbake to check image build folder in use?
http://www.yoctoproject.org/docs/current/bsp-guide/bsp-guide.html#customizing-a-recipe-for-a-bsp
Q2: How to change IMAGE_FEATURES setting? I would change splash variables.
http://www.yoctoproject.org/docs/current/poky-ref-manual/poky-ref-manual.html#ref-features-image
Hi Thomas,
The right way is to create a layer for your customizations so it is easy to maintain it in future so:
R1: add it in your layer
R2: create an image for your project.
Does psplash accept a progress bar? Is there any reasonable psplash doc ?
For example fbsplash accept. You can send progress value through fifo file.
Yes, psplash does.
There is no doc about it but we can assist you, at O.S. Systems, if you need any help. We do have done several customizations for it for customers along these years.
The package responsable for the bootscreen is the psplash; you need to make a specific layer with your project changes and one of those will be the ones for psplash so you have your brand logo during initial boot.
Hi Otavio,
Check metas and psplash is located in sources/meta_fsl-arm/psplash.
And make-image-header.sh is located here as well. If possible to run the script and finish this job?
We don't have psplash customization in meta-fsl-arm so you need to base in the Poky one.
You should have a new layer for your company or product and put it there (psplash bbappend, your headers and like).
Hi Otavio,
Well, so try to build a minimal build to test as below progress. But error found. Wish a good idea for new layer build.
wget http://downloads.yoctoproject.org/releases/yocto/yocto-1.3/poky-danny-8.0.tar.bz2
tar xjf poky-danny-8.0.tar.bz2
cd poky-danny-8.0/
git clone git://git://github.com/Freescale/meta-fsl-arm.git -b danny
cd ..
source oe-init-build-env
change conf/local.conf to MACHINE ??= 'imx28evk'
bitbake -s core-image-minimal
Show error as below
********************
$ bitbake -s core-image-minimal
Loading cache: 100% |##############################################################################################################| ETA: 00:00:00
Loaded 66 entries from dependency cache.
Parsing recipes: 100% |####################################| ETA: 00:00:00
Parsing of 859 .bb files complete (61 cached, 798 parsed). 1169 targets, 65 skipped, 0 masked, 0 errors.
ERROR: No recipes available for:
/home/thomas/yocto/poky-danny-8.0/meta-fsl-arm/recipes-qt/qt4/qt4-embedded_4.8.4.bbappend
/home/thomas/yocto/poky-danny-8.0/meta-fsl-arm/recipes-multimedia/gstreamer/gst-plugins-gl_0.10.3.bbappend
/home/thomas/yocto/poky-danny-8.0/meta-fsl-arm/recipes-qt/qt4/qt4-x11-free_4.8.4.bbappend
/home/thomas/yocto/poky-danny-8.0/meta-fsl-arm/recipes-graphics/mesa/mesa-dri_9.0.2.bbappend
ERROR: Command execution failed: Exited with 1
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
Your meta-fsl-arm is at master branch, not danny.
Please use the Yocto Project GIT server: meta-fsl-arm - Layer containing Freescale ARM hardware support metadata