YOCTO Project Build issue i.MX6DL- populate_sdk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

YOCTO Project Build issue i.MX6DL- populate_sdk

1,739件の閲覧回数
Chandrashekhar_MVE
Contributor III

Hi,

We are facing an issue with populate SDK build.

We are successfully bitbake .

  • DISTRO=fsl-imx-xwayland MACHINE=imx6dlsabresd source imx-setup-release.sh -b build-xwayland
  • bitbake imx-image-full

But when we try to do populate SDK we have error as attached. below are the commands,

  • bitbake -c populate_sdk imx-image-full

In short errors are with,

  • /meta-qt6/recipes-qt/qt6/qtopcua_git.bb:do_install_ptest_base
  • /meta-openembedded/meta-oe/recipes-kernel/spidev-test/spidev-test.bb:do_install

Rgds

Chandra

0 件の賞賛
返信
1 返信

1,555件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Is probably that you have not include the correct package for build yocto, or please erase everything and re-build again.

 

Regards

0 件の賞賛
返信