Xen hypervisor with AGL and Android Automotive

cancel
Showing results for 
Search instead for 
Did you mean: 

Xen hypervisor with AGL and Android Automotive

539 Views
vinothkumars
Senior Contributor IV
We are working on to port Xen hypervisor to the custom board with AGL as host and Android Automotive as Guest. We also need communication between the AGL and AA OS
 
Is that possible or do we need port Linux as host and AGL, AA as two guest OS?
 
Please suggest we need to initiate the design and proceed accordingly we believe AGL as host should be possible in that way we can also avoid one more OS footprint but we arent experts on this
Regards,
Vinothkumar Sekar
0 Kudos
2 Replies

378 Views
ruisb
Contributor I

Hi Vinothkumars

I have the same question with you. Are you able to run AGL on Xen hypervisor as dom0 now? I need your experience!

Thanks in advance

Shibo

0 Kudos

534 Views
Qmiller
NXP Employee
NXP Employee

AGL is not in support list of i.MX8QM .If you port it on i.MX8QM, you will meet lots of issues.

0 Kudos