Xen Hypervisor not working with Android image - iMX8QuadMax

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Xen Hypervisor not working with Android image - iMX8QuadMax

ソリューションへジャンプ
1,769件の閲覧回数
ranjith1
Contributor I

Hi Team

We are using IMX8 Quad max board. We have downloaded "L_VIRT_4.14.98_2.0.0_4.11_0.10_ga_images_MX8QMMEK" image to the board and made SD card partitions as per document. We have downloaded the android OS image "android_p9.0.0_2.3.5-auto_image_8qmek" from NxP website and loaded to SD card.

From U boot if we run the command "xenmmcboot" getting errors.

lsio_gpio1 [200] not owned by curr partition

Error: lsio_gpio1 Power up failed! (error =4)

lsio_gpio1 [200] not owned by curr partition

Error: lsio_gpio1 Power up failed! (error =4)

 

Please let us know how to resolve these errors.

 

Also let us know is there any other OS/RTOS can be run on Xen hypervisor which is supported by iMX8QuadMax?

 

Best Regards

Ranjith Kumar

0 件の賞賛
返信
1 解決策
1,754件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

It looks like PMIC is not completely build in the image or it is failing, i bet may try again.

For mx8QM we have the jailhouse and XEN hypervisor. where you can boot linux, windows, android, Winriver OS.

 

regards

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,755件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

It looks like PMIC is not completely build in the image or it is failing, i bet may try again.

For mx8QM we have the jailhouse and XEN hypervisor. where you can boot linux, windows, android, Winriver OS.

 

regards

0 件の賞賛
返信
1,706件の閲覧回数
ranjith1
Contributor I

Hi Team

Will Promox hypervisor will be supported by iMX8QM.

 

Best Regards

Ranjith Kumar 

0 件の賞賛
返信
1,745件の閲覧回数
ranjith1
Contributor I

Hi

Thanks for the reply.

There was an issue with the switch3 which should be on while downloading.

Now we are able to boot Android OS without errors.

 

Best Regards

Ranjith Kumar

0 件の賞賛
返信
1,002件の閲覧回数
vivektol
Contributor I

Hello Rajith,

 

Can you provide me this file /etc/xen/domu-imx8qm-mek-androidauto.cfg  for running Android as domu in imx8 board

 

0 件の賞賛
返信