Xen Hypervisor Deployment on SD Card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Xen Hypervisor Deployment on SD Card

1,003 Views
nevozade
Contributor IV

Hello,

I am following the application note AN13138 Xen Deployment on Layerscape Platforms (attached to this issue) to generate Xen hypervisor image and other needed files that work on imx8qm board. I completes the section 2.1 Build by following through the instructions here successfully and I generated the desired files in the desired directory.

However, in the section 2.2 Deployment, there are some tftp commands that should be given on u-boot but because of some problems, I cannot use the tftp properly and I do want to deploy xen hypervisor by using a SD card. Is it possible to load xen_addr, image, device tree blob etc. with SD card and if yes, how?

I would be very grateful if you could help me with running Xen and Dom0.

 

Regards.

Tags (4)
0 Kudos
Reply
1 Reply

978 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello

 

You may following the yocto user guide document section 5.6.11 to build xen. This is for layerscape not necessarily works for MX8QM.

 

regards

0 Kudos
Reply