Xen Hypervisor Deployment on IMX8 Quad Max

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Xen Hypervisor Deployment on IMX8 Quad Max

2,528件の閲覧回数
nevozade
Contributor IV

Hello,

I am trying to run Xen hypervisor on the imx8qm board. I am following the instructions on the AN13138 Xen Deployment on Layerscape Platforms application note. First, I did all instructions for the building phase (section 2.1) and I get all necessary generated files as expected:

-fsl-image-networking-imx8qmmek-20221011063852.rootfs.cpio.gz

-fsl-image-networking-imx8qmmek-20221011063852.rootfs.ext2

-fsl-imx8qm-mek.dtb

-Image

-xen-imx8qmmek

However, there is no u-boot file in the deploy folder and I load an external u-boot and cannot perform the TFTP commands which the application note uses in the section 2.2 Deployment. I run 'run xenmmcboot' command in u-boot but because of the TFTP failure, I encounter with some fdt address errors. I would be very grateful if you could help me by explaining the TFTP part with which u-boot file. Briefly, can anyone helps to run Dom0 and create new DomU s?

 

Regards.

ラベル(1)
タグ(4)
1 返信

2,501件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Please refer to the Chapter 12 in Linux User's guide (ver. L5.4.70_2.3.0).

And the section 5.6.11 in i.MX Yocto User's guide.

Please download the documentation from here: Documentation

タグ(1)
0 件の賞賛
返信