XIO fatal IO error 22

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

XIO fatal IO error 22

3,031 Views
i_ashok_s
Contributor I

Hi, I am running 'gstreamer' on iMX6Q Sabrelite (Ubuntu Bionic) interfaced USB camera like....


$GSTL v4l2src device=/dev/video1 ! 'video/x-raw, format=(string)UYVY,width=640,height=480,framerate=(fraction)30/1' ! autovideosink

I got this error message:

XIO: fatal IP errro 22 (Invalid argument) on X server ":0"

         after 8 requests (8 known processed) with 0 events remaining.

 

Please suggest the solution. Thanks

0 Kudos
Reply
3 Replies

3,014 Views
Bonnell_B
Contributor I

Thanks for the information targetehr.

0 Kudos
Reply

3,024 Views
igorpadykov
NXP Employee
NXP Employee

Hi i_ashok_s

 

for sabrelite gstreamer examples one can look at

https://boundarydevices.com/yocto-dunfell-release-for-i-mx6-i-mx7-platforms/

https://boundarydevices.com/wiki/bd-sl-imx6/

 

Best regards
igor

0 Kudos
Reply

2,995 Views
i_ashok_s
Contributor I

Thanks @igorpadykov for your suggestion.

I am working on it but nothing happens when I tried to run this command.
gst-launch-1.0 playbin uri=file:///home/Desktop/Hobbit-1080p.mov video-sink=imxipuvideosink

 
 

GSt-imx.JPG

 

I cant see any other window playing the file.

Seems 

 

 

0 Kudos
Reply