XHCI USB3.0 recognition Issues

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

XHCI USB3.0 recognition Issues

744 次查看
MasakiHayakawa
Contributor III

Hi,

I am having some issues with a TI USB 3.0 hub.
I have a TUSB7320 USB 3.0 hub connected through PCIe.
Three usb storages are recognized at super speed, but I can't get any message when insert or remove to the other four.
When these are not recognized, mx6-pcie-msi and xhci_hcd interrupts are not work.
My kernel config is set by i.MX_Linux_Reference_Manual.pdf 40.4 Using PCIe Endpoint and Running Tests.
Could you advice me ?
Software:
I've used fsl-yocto-L4.1.15_1.0.0-ga.
Hardware:
i.MX6SX custom board
0 项奖励
回复
0 回复数