X11/vivante_drv crash on Kernel 3.10.17

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

X11/vivante_drv crash on Kernel 3.10.17

2,287 Views
tomd_
Contributor II

Hi all,

I'm using the newest meta-fsl-arm branch (master-next) and yocto in order to build an image for my imx6dl based on the 3.10.17 kernel.

Build went through and boots. Everything looks fine until I do start my X-server. The system crashes/freezes while loading the extension 'vivext'

I'm sure that the build includes the correct recipes to provide the GPU/VPU support:

- kernel-3.10.17-1.0.0-beta+gec1af9f;3.10.17

- imx-lib;3.10.17-1.0.0

- libegl-mx6;3.10.17-1.0.0-hfp

- libgal-mx6;3.10.17-1.0.0-hfp

- libgl-mx6;3.10.17-1.0.0-hfp

- libgles2-mx6;3.10.17-1.0.0-hfp

- libglslc-mx6;3.10.17-1.0.0-hfp

- libvpu4;3.10.17-1.0.0

- xf86-video-imxfb-vivante;3.10.17-1.0.0

Any ideas?

Log output:

root@imx6dlsabresd:/etc/X11# ./Xserver

tslib: /dev/input/touchscreen0

exec xinit /etc/X11/Xsession -- /usr/bin/Xorg -br -pn  -dpi 100

X.Org X Server 1.14.4

Release Date: 2013-10-31

X Protocol Version 11, Revision 0

Build Operating System: Linux 3.11.0-14-generic x86_64

Current Operating System: Linux imx6dlsabresd 3.10.17-1.0.0_beta+gec1af9f #1 SMP Mon Feb 3 16:10:03 CET 2014 armv7l

Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk0p2 rootwait rw

Build Date: 03 February 2014  04:34:46PM

Current version of pixman: 0.32.4

        Before reporting problems, check http://wiki.x.org

        to make sure that you have the latest version.

Markers: (--) probed, (**) from config file, (==) default setting,

        (++) from command line, (!!) notice, (II) informational,

        (WW) warning, (EE) error, (NI) not implemented, (??) unknown.

(==) Log file: "/var/log/Xorg.0.log", Time: Thu Jan  1 00:01:02 1970

(==) Using config file: "/etc/X11/xorg.conf"

(==) Using system config directory "/usr/share/X11/xorg.conf.d"

Initializing built-in extension Generic Event Extension

Initializing built-in extension SHAPE

Initializing built-in extension MIT-SHM

Initializing built-in extension XInputExtension

Initializing built-in extension XTEST

Initializing built-in extension BIG-REQUESTS

Initializing built-in extension SYNC

Initializing built-in extension XKEYBOARD

Initializing built-in extension XC-MISC

Initializing built-in extension XFIXES

Initializing built-in extension RENDER

Initializing built-in extension RANDR

Initializing built-in extension COMPOSITE

Initializing built-in extension DAMAGE

Initializing built-in extension MIT-SCREEN-SAVER

Initializing built-in extension DOUBLE-BUFFER

Initializing built-in extension DPMS

Initializing built-in extension X-Resource

Initializing built-in extension XVideo

Initializing built-in extension XVideo-MotionCompensation

Initializing built-in extension XFree86-VidModeExtension

Initializing built-in extension XFree86-DGA

Initializing built-in extension XFree86-DRI

Initializing built-in extension DRI2

Loading extension GLX

Loading extension vivext

Labels (1)
7 Replies

1,146 Views
tomd_
Contributor II

I found the problem:

I was building my image with wrong u-boot. I was using the 'u-boot-fslc' instead of 'u-boot-imx'. Adding the following preferred provider in the local.conf has solved my problem:

PREFERRED_PROVIDER_u-boot = "u-boot-imx"
PREFERRED_PROVIDER_virtual/bootloader = "u-boot-imx"

1,146 Views
OtavioSalvador
Senior Contributor II

In fact the problem is that U-Boot mainline lacks support for the PMIC and we need to use the -ldo device tree. Please give it a try and confirm if it solves your issue as well.

Using the u-boot-imx is another solution as it provides the PMIC and LDO bypass support. But I always prefer to stay close to mainline :smileywink:

1,146 Views
tomd_
Contributor II

Otavio, thanks for your advice. I have tested my setup with the 'uboot-fslc' and the ldo dtb:

I have just modified my u-boot variable from

fdt_file=imx6dl-sabresd.dtb

to

fdt_file=imx6dl-sabresd-ldo.dtb (setenv fdt_file 'imx6dl-sabresd-ldo.dtb')

This has fixed the issue as well. So it makes sense to stick with the mainline u-boot. Thanks alot!

0 Kudos
Reply

1,146 Views
fabio_estevam
NXP Employee
NXP Employee

Tom,

Please send this changes as a patch to meta-fsl-arm if you have a chance.

Regards,

Fabio Estevam

0 Kudos
Reply

1,146 Views
LeonardoSandova
Specialist I

Hi Tom, actually you only need one on those lines. I will keep the second and remove the first.

0 Kudos
Reply

1,146 Views
tomd_
Contributor II

Thanks for the feedback, I will keep the second line :smileywink:

0 Kudos
Reply

1,146 Views
LeonardoSandova
Specialist I

Please ignore my previous recommendation. Seems that both statements are needed :smileyhappy: Sorry for the noise. The interesting point I can get from this is that kernel just needs one (PREFERRED_PROVIDER_virtual/kernel="linux-imx") so I was indeed biased by this fact...

0 Kudos
Reply