Hello,
I am trying to run X11 examples included in gpu_sdk_v1.00 package. I am using Yocto fsl-gui-image. I have tried to run 06_Texturing example under GLES2.0 folder. I have only modified -mfloat-abi variable in the Makefile from softfp to hard. Then I have compiled the code, but unfortunately it is not running on IMX.6 board. I got the following error message when I try to run ./06_Texturing;
06_Texturing: ../common/src/fsl_egl.c:51 fsl_getNativeDisplay: Assertion 'eglNativeDisplayType != ((void *)0)' failed
Aborted.
What can be wrong? It seems that there is a problem at XOpenDisplay function which is called by fsl_getNativeDisplay function. Is there anything to be done to enable X11? I checked that the libraries are loaded under /usr/libç What should I do?
Thanks&Best Regards,
Fikret
已解决! 转到解答。
To fix the X11 issues, Please try,
$ modprobe galcore
and display setting
$ export DISPLAY=:0.0
Regards