X11 imx53qsb Xorg.conf Qt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

X11 imx53qsb Xorg.conf Qt

962件の閲覧回数
GiulioBenetti
Contributor I

Hi all,

was anybody able to make X11 work with imx accelerated framebuffer driver?

Using Xfbdev+Matchbox and Qt I have poor performances.

Example:

on Qt I use 1 superclass child of QWidget.

After I create 10 different QWidget childs where I have a lot of png.

This make it very slow.

Instead If I use 10 different QWidgets separated it works faster, but I have problem with background.

If one widget is smaller than the one in background it paints black background.

What can I do?

Does Xorg solve performance issue?

Or maybe there is a workaround?

Thanks in advance.

タグ(1)
0 件の賞賛
返信
0 返答(返信)