X11 forwarding on imx8mp-evk with xwayland

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

X11 forwarding on imx8mp-evk with xwayland

1,371 Views
axjensen
Contributor I

Hi,

 

We are unable to get X11 forwarding on imx8mp-evk with xwayland.

xauth is added to xwayland and sshd set up to allow X11 forwarding

We are trying to execute an application as root.

Doing an ssh connection as root with X11 Forwarinng we launch an application from the terminal.

The GUI of the application  then is displayed on the monitor attached to the imx8mp and not forwarded over SSH.

 

What might be the problem?

 

 

0 Kudos
Reply
2 Replies

1,339 Views
joanxie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

1,325 Views
axjensen
Contributor I

Thank you @joanxie 

As I mention in the original message, xauth is already installed.

I've have also tried the advices from you two last links, which does not solve the problem. So I am stuck.

In your first link, a user @OtavioSalvador has successfully solved the problem by configuring OpenSSH. It would be of great help to know what he had to change from default values.

 

Thank you,

 

 

0 Kudos
Reply