X11 Error in imx6ull

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

X11 Error in imx6ull

1,743 Views
sheraz_ali
Contributor II
When runnong Application via mono We get the following x11 Error
X11 Error encountered:
  Error: BadMatch (invalid parameter attributes)
  Request:     1 (0)
  Resource ID: 0x1600082
  Serial:      2228
  Hwnd:        Hwnd, Mapped:False ClientWindow:0x1600083, WholeWindow:0x1600082, Zombie=False, Parent:[Hwnd, Mapped:False ClientWindow:0x1600011, WholeWindow:0x1600010, Zombie=False, Parent:[<null>]]
  Control:     <handle 1600083 non-existant>  at System.Environment.get_StackTrace () [0x00000] in <99b7767fda36428caf8c4eed0d54aaec>:0
X11 Error encountered:
  Error: BadWindow (invalid Window parameter)
  Request:     2 (0)
  Resource ID: 0x1600083
  Serial:      2230
  Hwnd:        Hwnd, Mapped:False ClientWindow:0x1600083, WholeWindow:0x1600082, Zombie=False, Parent:[Hwnd, Mapped:False ClientWindow:0x1600011, WholeWindow:0x1600010, Zombie=False, Parent:[<null>]]
  Control:     <handle 1600083 non-existant>  at System.Environment.get_StackTrace () [0x00000] in <99b7767fda36428caf8c4eed0d54aaec>:0
 
X11 Error encountered:
  Error: BadDrawable (invalid Pixmap or Window parameter)
  Request:     55 (0)
  Resource ID: 0x1600083
  Serial:      2249
  Hwnd:        Hwnd, Mapped:False ClientWindow:0x1600083, WholeWindow:0x1600082, Zombie=False, Parent:[Hwnd, Mapped:False ClientWindow:0x1600011, WholeWindow:0x1600010, Zombie=False, Parent:[<null>]]
  Control:     OpenTK.GLControl  at System.Environment.get_StackTrace () [0x00000] in <99b7767fda36428caf8c4eed0d54aaec>:0
Labels (3)
0 Kudos
Reply
2 Replies

1,664 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello sheraz,

This errors is fixed in latest BSP, Also this errors correspond to X11.

Regards

0 Kudos
Reply

1,664 Views
sheraz_ali
Contributor II

How to fix the issue using yocto

Currently i am using krogoth branch.

0 Kudos
Reply