X-11 is supported on IMX8mq

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

X-11 is supported on IMX8mq

2,012 Views
sim_guo
Contributor I

If i want the X-11 is supported on the IMX8mq, what needs to be done?

Tags (2)
0 Kudos
Reply
4 Replies

1,902 Views
sim_guo
Contributor I

I tried to use xwayland to be compatible with X11, but it didn't work due to an EGL error.
If i use Weston directly, his features are not powerful enough. Is there any other desktop system to support Wayland's , such as the genome. . .

0 Kudos
Reply

1,902 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

So sorry about that

You can see that in our newest BSP

• No X11 backend is supported in i.MX 8MQuad.
• No Frame Buffer backend is supported in i.MX 8MQuad

Hope this can do help for you.

Have a nice day

Rita

0 Kudos
Reply

1,902 Views
sim_guo
Contributor I

We want a desktop system similar to xfce, kde and the like. Based on imx8mq, 4.14.78. Is there any solution?

we didn’t choose weston because it’s too simple.

0 Kudos
Reply

1,902 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Or if you want to try the ubuntu that our third party make:

https://boundarydevices.com/wiki/ubuntu-for-nitrogen8/ 

0 Kudos
Reply