Windows 10 IoT on NXP iMX8MP with 8GB RAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Windows 10 IoT on NXP iMX8MP with 8GB RAM

2,064件の閲覧回数
Ben10
Contributor II

Will Windows 10 IoT work on NXP iMX8MP based custom board based having 8GB RAM? 

Our board boots with Windows 10 IoT when we mention "giMX8TokenSpaceGuid.PcdBank1MemorySize" as 3GB. When we mention "giMX8TokenSpaceGuid.PcdBank1MemorySize" as 5GB, it doesn't work.

 

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

2,022件の閲覧回数
Ben10
Contributor II

Hi Mike,

We have already tried what has been done in the patch file, but it doesn't work for us, the Windows is stuck in the Windows logo stage, the Windows installation is not happening.

Regards,

Benz Samuel

0 件の賞賛
返信

2,011件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer my reply at case# 00673030.

Thank you for the understanding.

Mike

0 件の賞賛
返信

2,023件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

We would recommend customer to check the setting according to attached patch file.

And please also refer below config for a stable 8GB RAM as reference:

mu_platform_nxp/NXP/MX8QXP_MEK/Drivers/SmbiosPlatformDxe/SmbiosPlatformDxe.c

// Memory device
STATIC CONST ARM_TYPE17 mArmDefaultType17 = {
  {
    { // SMBIOS_STRUCTURE Hdr
      EFI_SMBIOS_TYPE_MEMORY_DEVICE, // UINT8 Type
      sizeof (SMBIOS_TABLE_TYPE17),  // UINT8 Length
      SMBIOS_HANDLE_DRAM,
    },
    SMBIOS_HANDLE_MEMORY, //array to which this module belongs
    0xFFFE,               //no errors
    0xFFFF, // unknown total width
    0xFFFF, // unknown data width
    0x2000, // 8GB

 Below is the test result: 

Hui_Ma_0-1734511418188.png

Wish it helps.

Mike

0 件の賞賛
返信