Windows 10 IoT Enterprise with GPIO Controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Windows 10 IoT Enterprise with GPIO Controller

2,608 Views
hankwang
Contributor V

Hello, I have a GPIO as an output pin that I need to control. I want to know how to control it. Do you have any demo utilities or sample code?

My CPU is 8M Plus.  This pin needs to be controlled. you can refer the attached file.

 

Labels (1)
0 Kudos
Reply
5 Replies

1,458 Views
gerfen
Contributor I

@Manuel_Salas  I'm in the same boat WRT to the need to control GPIO.  Can you send me a copy of the GPIO tool please?  Thanks!

0 Kudos
Reply

2,563 Views
hankwang
Contributor V

Hello, is there any update?

0 Kudos
Reply

2,550 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @hankwang 

 

I sent you a direct message. I will re-send to you.

 

Best regards.

 

Salas.

0 Kudos
Reply

2,353 Views
aber
Contributor III
Hi Alejandro_Salas
I also encountered the same problem, can you send me a copy? thanks!
0 Kudos
Reply

2,545 Views
hankwang
Contributor V

Hi @Manuel_Salas  Got it... This tool can switch GPIO levels to high or low. The GPIO tool is good.