Windows 10 IoT : Amount of RAM usable in 8MPLUSLPD4-EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Windows 10 IoT : Amount of RAM usable in 8MPLUSLPD4-EVK

跳至解决方案
3,167 次查看
hiron
Contributor II

I am now evaluating Windows 10 IoT W1.1.0, 6/2022 BSP release and successfully bring up the Windows 10 IoT GUI using 8MPLUSLPD4-EVK.

My question is for amount of RAM recognized and usable. In Performance tab of task manager states there's 6GB of RAM recognized, but total 2.7 GB of RAM appears usable.

Is this the limitation for current W1.1.0 BSP release? Or is there any easy means to utilize full of installed RAM?

Thanks,

PLUS_DESKTOP_memory.png

 

 

标记 (2)
0 项奖励
回复
1 解答
3,158 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello hiron,

The Win10IoT just work with 3 GB ram, this a defect in WinIot sorry, you have to wait until next relase appears.

Regards

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,642 次查看
ChrisChang1234
Contributor III

Hi:

I'm using BSP 1.4.1 for a 8GB-DDR board.

And the problem is still there.

How to fix it?

 

 

0 项奖励
回复
3,155 次查看
hiron
Contributor II

OK I understand.

I will check next BSP release, may be in September timeframe, thanks!

 

0 项奖励
回复
3,093 次查看
anthonychen-msft
Contributor II

There's a HW bug in the USB controller on the 8M Plus that causes issues for the Windows IoT OS when more than 3GB of RAM is enabled. There's a workaround to this issue being made in the Windows IoT OS which will be available in an upcoming Windows IoT OS update. Once this OS update is available, we'll have the user guide and default scripts updated to use all 6GB instead of limiting to 3GB. 

0 项奖励
回复
3,159 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello hiron,

The Win10IoT just work with 3 GB ram, this a defect in WinIot sorry, you have to wait until next relase appears.

Regards

0 项奖励
回复
2,288 次查看
Alex_Chang_633
Contributor III

Hi @Bio_TICFSL ,

Does this problem still exist in W21H2-1-5-0-imx-windows-bsp-binaries.zip?

When we boot up i.MX8M Quad EVK, we can see DRAM: 4 GiB in the U-Boot debug log.

But when we boot up into Microsoft Windows 10 21H2 LTSC 64-bit operating system, the installed physical memor only has 3 GB.

We would like to know, is our problem the same with this article?

Thanks for you and NXP Teams help.

0 项奖励
回复