Windows 10 IOT core BSP with i.MX8M mini EVK

cancel
Showing results for 
Search instead for 
Did you mean: 

Windows 10 IOT core BSP with i.MX8M mini EVK

451 Views
Contributor I

Hi,

Windows 10 IOT core stops booting up after showing windows logo with i.MX8M mini EVK.

But when a USB device is connecting to USB OTG (Type-C) port from power-on the EVK, it can boot up correctly.

Is this an expected phenomenon?

BR,

Junichi

Labels (1)
0 Kudos
2 Replies

62 Views
Contributor I

Dear support team,

>Anyway, it is recommended verify the board connections, according with the “Get Started with the i.MX 8M Mini EVK” page.

There is no description to connect a USB device to Type-C port in that document.

GitHub - ms-iot/imx-iotcore at imx-iotcore-v1.0.0 

According to the URL above, there is a description below.

https://github.com/ms-iot/imx-iotcore/tree/imx-iotcore-v1.0.0

pastedImage_5.png

So I posted this question to NXP community.

BR,

Junichi

0 Kudos

62 Views
NXP Employee
NXP Employee

Hi Junichi,

In case of the Windows related questions, please use the Microsoft Community.

Anyway, it is recommended verify the board connections, according with the “Get Started with the i.MX 8M Mini EVK” page.

 

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 Kudos