Hi,
Windows 10 IOT core stops booting up after showing windows logo with i.MX8M mini EVK.
But when a USB device is connecting to USB OTG (Type-C) port from power-on the EVK, it can boot up correctly.
Is this an expected phenomenon?
BR,
Junichi
Dear support team,
>Anyway, it is recommended verify the board connections, according with the “Get Started with the i.MX 8M Mini EVK” page.
There is no description to connect a USB device to Type-C port in that document.
GitHub - ms-iot/imx-iotcore at imx-iotcore-v1.0.0
According to the URL above, there is a description below.
https://github.com/ms-iot/imx-iotcore/tree/imx-iotcore-v1.0.0
So I posted this question to NXP community.
BR,
Junichi
Hi Junichi,
In case of the Windows related questions, please use the Microsoft Community.
Anyway, it is recommended verify the board connections, according with the “Get Started with the i.MX 8M Mini EVK” page.
Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------